How to build a CodeWarrior project using codes  generated by toolbox

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to build a CodeWarrior project using codes  generated by toolbox

2,562件の閲覧回数
hjhjhj
Contributor III

Hi,

     I want to  build a MPC5643L CodeWarrior project using codes  generated by toolbox,   but there're some errors I never met .Can anybody give me some suggestions to configured the CodeWarrior project?

 

Thank you!

Hj

Original Attachment has been moved to: can_simple_block_rappid_rtw.rar

0 件の賞賛
返信
4 返答(返信)

2,331件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hi,

It would be really faster for you if you could specify the compiler errors here.

Peter

0 件の賞賛
返信

2,330件の閲覧回数
hjhjhj
Contributor III

Hi Peter,

     The attachment is the simulink model and the codes generated by the model.

170618.PNG

Thank you !

Hj

0 件の賞賛
返信

2,330件の閲覧回数
martin_kovar
NXP Employee
NXP Employee

Hello,

I posted you the answer in thread below:

https://community.nxp.com/thread/453687 

Regards,

Martin

0 件の賞賛
返信

2,330件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hi,

You are using BOOKE instructions in section which is targeted to be VLE.

Reword it to VLE or dissable VLE and leave them as BOOKE.

Peter

0 件の賞賛
返信