How to Inject 2b SRAM ECC ERROR On MPC5744P

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to Inject 2b SRAM ECC ERROR On MPC5744P

3,185 Views
jasoncao
Contributor II

Hi,

     To test my ECC error handler,I want to inject 2b SRAM ECC error on mpc5744p.I had read the AN5200,but there isn't ECSM module in MPC5744P.Anyone could help me?

Thank you very much!

Labels (1)
0 Kudos
Reply
4 Replies

2,544 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

Instead of ECSM, there is EIM (Error Injection Module).

Currently I made two examples, one is for MPC5777C device that uses EIM and ERM modules (showing RAM ECC injections), second is from MPC5744P device that uses EIM and MEMU modules (showing FLASH ECC injections):

Example MPC5777C-1b+2b_RAM_ECC_error_injection GHS614

Example MPC5744P_1b+2b_FLASH_ECC_error_injection GHS614

With combination of both it should be possible to create RAM ECC injection with using of EIM and MEMU modules on MPC5744P. I plan to do it myself when I have time for it.

0 Kudos
Reply

2,544 Views
jasoncao
Contributor II

Hi David,

     I had try to modify the 'Example MPC5777C-1b+2b_RAM_ECC_error_injection GHS614' to inject 2b RAM ECC in MPC5744P.There is some different betwen MPC5777C EIM and MPC5744P EIM.But I didn't succeed.

     The code as below:

static vuint32_t test[2] __attribute__ ((aligned (8))) =

{

    0xBABADEDA,

    0xABBAABBA

};

void Generate_noncorrectable_ECC_error(void)

{

    register vuint32_t test_read = 0;

    /* invert 2 LSB bits to create non-correctable data error */

    EIM.EICHD_Word1.R = 0x00000003;

    /* PRAMC_0 channel error injection enable */

    EIM.EICHEN.R = 0x80000000;

    /* global error injection enable */

    EIM.EIMCR.R = 1;

    /* error caused by read (it should set MCSR[MAV, LD, BUS_DRERR]) */

    test_read = test[0];

}

0 Kudos
Reply

2,544 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

It is otherwise. By MPC5744P's EIM module you can inject ECC fault only to transfer control descriptor of eDMA (that is peripheral RAM).

pastedImage_0.png

I am not sure if it is possible to inject ECC fault into system RAM on MPC5744P, probably it is not. Let me yet examine.

0 Kudos
Reply

2,544 Views
jasoncao
Contributor II

Hi David,

     Thank you very much! Waiting for your good news.LoL

0 Kudos
Reply