Example MPC5744P_1b+2b_FLASH_ECC_error_injection GHS614

File uploaded by David Tosenovjan Employee on Mar 4, 2016Last modified by David Tosenovjan Employee on Apr 27, 2016
Version 3Show Document
  • View in full screen mode

********************************************************************************

* Detailed Description:

* Purpose of the example is to show how to generate Multi-bit or Single-bit

* ECC error in internal FLASH (user must choose it in the option at the end of

* main function).

* Flash over-programming is used to generate a non-correctable (or single-bit)

* ECC error in FLASH. The bad data is accessed then what's generate IVOR1

* exception or FCCU_Alarm_Interrupt. Both function calls MEMU handler.

* Example also offers useful macros for MEMU module.

* The example displays notices in the terminal window (connector J19 on

* MPC57xx_Motherboard)(19200-8-no parity-1 stop bit-no flow control on eSCI_A).

* No other external connection is required.

* ------------------------------------------------------------------------------

* Test HW:         MPC57xx_Motherboard + MPC5744P-144DC

* MCU:             PPC5744PFMLQ8,0N15P,QQAA1515N, Rev2.1B

* Fsys:            200 MHz PLL with 40 MHz crystal reference

* Debugger:        Lauterbach Trace32

* Target:          internal_FLASH, RAM

* Terminal:        19200-8-no parity-1 stop bit-no flow control

* EVB connection:  default

********************************************************************************

Outcomes