How to BlinkLED sample project on MPC5748G

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to BlinkLED sample project on MPC5748G

Jump to solution
3,392 Views
jzhang1
Contributor II

I'm learning the example project of BlinkLED. And it runs well. However, the example is to make LED2 blink, then I'm trying to modify the code to make other LED blinking. (let's say LED1 as an example)

Original Code:(same as a tutorial)

   void pitCh0Handler(void){

      PIT_DRV_ClearStatusFlags(INST_PIT1, 0U);        /* Clear PIT channel 0 interrupt flag */
      SIUL2->GPDO[0] ^= SIUL2_GPDO_PDO_4n_MASK;       / * Toggle LED (GPIO 0 connected to user LED 2) */
      }

   int main(void){

      CLOCK_DRV_Init(&clockMan1_InitConfig0);
      PINS_DRV_Init(NUM_OF_CONFIGURED_PINS, g_pin_mux_InitConfigArr);
      INT_SYS_InstallHandler(PIT_Ch0_IRQn, &pitCh0Handler, NULL);

      PIT_DRV_Init(INST_PIT1, &pit1_InitConfig);
      PIT_DRV_InitChannel(INST_PIT1, &pit1_ChnConfig0);
      PIT_DRV_StartChannel(INST_PIT1,0U);

   }

Modify area:

change pin mux to PA[4], which represents LED1.

SIUL2->GPDO[4] ^= SIUL2_GPDO_PDO_4n_MASK

 

Result: LED1 turns on, but never blink.

Does anyone know why?

I think the problem is "SIUL2_GPDO_PDO_4n_MASK", but I couldn't find any pin muxing in the MPC5748G datasheet!

No matter what I search ("SIUL", "GPDO", “GPDI”) inside the datasheet, I receive very limited information. Unlike MPC5744P datasheet, clear and helpful. Or am I looking at wrong data datasheet?

Please helps!

Labels (1)
Tags (1)
1 Solution
3,289 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

See the description of GPDO register. It's 32bit register which contains four bits to control four pins.

So, GPDO[0] covers GPIOs 0-3. GPDO[1] covers GPIOs 4-7 and so on...

To write PA[4], you need to write GPDO[1] using mask SIUL2_GPDO_PDO_4n_MASK.

(Note: this depends on used header file. Sometimes the GPDO is defined as array of 32bit registers like this, sometimes it's defined as array of 8bit registers, so it is more straightforward. Both options can be used.)

Anyway, if you use SDK, why not to use SDK functions for this? There are functions like PIN_DRV_WritePin, PIN_DRV_SetPins, PIN_DRV_ClearPins, PIN_DRV_TogglePins...

Regards,

Lukas

View solution in original post

4 Replies
3,289 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi Junyi,

description of the registers and pin muxing can be found in the reference manual:

https://www.nxp.com/webapp/Download?colCode=MPC5748GRM 

There's an excel file attached inside the document:

pastedImage_2.png

Regards,

Lukas

0 Kudos
Reply
3,289 Views
jzhang1
Contributor II

Lukas,

Thank you for your reply.

I found the excel, but it didn't solve my question.

For LED2[PA0]:

SIUL2_GPDO_PDO_4n_MASK = 0x01000000

then how to map the LED1[PA4]? To make it turn on?

Thanks.

0 Kudos
Reply
3,290 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

See the description of GPDO register. It's 32bit register which contains four bits to control four pins.

So, GPDO[0] covers GPIOs 0-3. GPDO[1] covers GPIOs 4-7 and so on...

To write PA[4], you need to write GPDO[1] using mask SIUL2_GPDO_PDO_4n_MASK.

(Note: this depends on used header file. Sometimes the GPDO is defined as array of 32bit registers like this, sometimes it's defined as array of 8bit registers, so it is more straightforward. Both options can be used.)

Anyway, if you use SDK, why not to use SDK functions for this? There are functions like PIN_DRV_WritePin, PIN_DRV_SetPins, PIN_DRV_ClearPins, PIN_DRV_TogglePins...

Regards,

Lukas

3,289 Views
jzhang1
Contributor II

Thanks!!!

GPDO[1] works! "SIUL2->GPDO[1] ^= SIUL2_GPDO_PDO_4n_MASK;"

I try to use function "PIN_DRV_TogglePins" to replace the mask(which I'm not familiar with), I found it is much easier for me to achieve the same result. 

"PINS_DRV_TogglePins(PTA,1<<4);"

Again, Thank you for your help.

0 Kudos
Reply