Getting started with exceptions?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Getting started with exceptions?

2,233 Views
bobgrimes
Contributor II

The MCP5744P is cool, but the docs are really confusing for someone jumping into the deep end...  For me, I think the biggest problem is terminology; I've been working the embedded processing scene for many years, but until now, I have only encountered Power architecture in Xilinx Virtex4.  This is the background I am coming from, so please understand that I understand the concepts here, but not the terminology; this is the cause of my confusion, I am sure.  To be clear, below when I "quote" something, this is to indicate where I think I am confused by terminology, or specifics of the 5744P.

I am trying to develop "exception handlers" for various issues that may arise.  A partial list I was given is this:

  • Critical Interrupt (IVOR0)
  • Machine Check (IVOR1)
  • Data Storage (IVOR2)
  • Instruction Storage (IVOR3)
  • Alignment (IVOR5)
  • Program (IVOR6)

Here are my problems that are causing great, personal grief, that I am 1000% positive many out there can help with!

  1. Where the hell do I find documentation for these???
  2. How do I associate a handler for these?  I'm not looking for the basics of how one writes an ISR or the like.  I just don't know the details of how you wire one up to the "exception".  For example, using other architectures, how do I set an interrupt vector to point to an ISR to service the interrupt?  How is it enabled?
  3. In the interest of testing my handlers, how do I intentionally cause any/all of these? 

To those in the know, my frustration lies in the fact that I know the information is out there, but the complexity and terminology differences between simpler (?) architectures (e.g. wicked old Intels, Coldfires, ARM) and this beast are killing my confidence!

2 Replies

1,936 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello Bob,

A1: You can find the documentation in core reference manual.MPC5744P contains 2x e200z425 core,

Here is link:http://cache.nxp.com/assets/documents/data/en/reference-manuals/e200z4RM.pdf?fsrch=1&sr=2&pageNum=1 

Refer to chapter 5 Interrupts and Exceptions, specially to Table 5-3. Exceptions and Conditions.

A2: I am not sure if there is a guide document for it but we have posted a lot of examples including Exception, ISR and handlers here on community:

MPC5 software example list 

A3:These details you can find in core reference manual in chapter 5.7 Interrupt Definitions.

Hope it helps,

Peter

0 Kudos
Reply

1,936 Views
bobgrimes
Contributor II

Hi Peter,

I want to thank you for your kind reply. Looking back, I'm rather

embarrassed at my post; chalk it up to frustration and pre-vacation

exhaustion. I was out this last week, so I'm just getting back in stride.

Immediately before my vacation, I did talk with a colleague who, I think,

got me over the hump on this issue, at least I hope so! The problem I

think I was having is simply too much detailed information, not enough

technical overview, and a terminology mismatch. For example, I already had

the documentation resources you provided; also, I had the examples too.

(I'm not discounting you providing them, thanks!)

The problem was this: I started with this example: (

https://community.nxp.com/docs/DOC-333754). I was able to compile and run

this on our debugger/hardware, so I was encouraged. However, when I ported

it to our system, I could not get the interrupts to fire. As far as I

could determine, everything is the same between the demo code and the

ported version. This had me very frustrated, and combined with a lack of

confidence that I understood anything about the chip, caused my post.

Turns out the issue is, as expected, both unrelated to getting a Machine

Check interrupt to fire, and specific to our system. I would explain more,

but it is a long story, and I think I am past the sticking point - though I

will know more in a few hours!

Thanks again, and best regards.

Bob

0 Kudos
Reply