FreeRTOS - MPC5748g - DevKit.

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

FreeRTOS - MPC5748g - DevKit.

4,851件の閲覧回数
Krishnaja
Contributor II

Hi,

To a "freertos_mpc5748g" example, I added a "linflexed_uart" component. And also created a task for linflexed_uart.
But I am not getting linflexed_ uart task output.

Krishnaja.

0 件の賞賛
返信
10 返答(返信)

4,814件の閲覧回数
Krishnaja
Contributor II

Hi Lukas,

I don't think timeout is an issue. Anyways I tried as you suggested by keeping the value to 3seconds. But it did not help.

I had created the return code for linflexed uart task, just below led task.

I am using S32 Design Studio for power Architecture Version2.1 .

Can you go through the code and tell me what I have missed.

 

Krishnaja.

 

0 件の賞賛
返信

4,826件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

isn't the timeout value of LINFLEXD_UART_DRV_ReceiveDataBlocking function too short?

What is the return code of this function? I can see you don't check it.

If this doesn't help, what is the version of SDK and S32DS?

Regards,

Lukas

 

 

0 件の賞賛
返信

4,760件の閲覧回数
Krishnaja
Contributor II

Any updates?? @lukaszadrapa 

タグ(1)
0 件の賞賛
返信

4,752件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

sorry for delay, we had Easter holidays here, so some answers are delayed.

Let me repeat this question to move forward - what is the return code from LINFLEXD_UART_DRV_ReceiveDataBlocking?

Regards,

Lukas

 

0 件の賞賛
返信

4,747件の閲覧回数
Krishnaja
Contributor II

 

Hi,

Let us keep receive Data block aside for time being. 

I have attached main of my code. According to high-lighted code, I should get "Hello world!" msg before the scheduler task on terminal. But I am not getting the same.

int main(void)
{


/* Write your local variable definition here */
/*** Processor Expert internal initialization. DON'T REMOVE THIS CODE!!! ***/
#ifdef PEX_RTOS_INIT
PEX_RTOS_INIT(); /* Initialization of the selected RTOS. Macro is defined by the RTOS component. */
#endif
/*** End of Processor Expert internal initialization. ***/
/* Initialize clocks */
CLOCK_SYS_Init(g_clockManConfigsArr, CLOCK_MANAGER_CONFIG_CNT,
g_clockManCallbacksArr, CLOCK_MANAGER_CALLBACK_CNT);
CLOCK_SYS_UpdateConfiguration(0U, CLOCK_MANAGER_POLICY_AGREEMENT);
PINS_DRV_Init(NUM_OF_CONFIGURED_PINS, g_pin_mux_InitConfigArr);
/* Initialize LINFlexD module for UART usage */
LINFLEXD_UART_DRV_Init(INST_LINFLEXD_UART1, &linflexd_uart1_State, &linflexd_uart1_InitConfig0);
/* Send the greeting message to console */
LINFLEXD_UART_DRV_SendData(INST_LINFLEXD_UART1, (uint8_t*)msg, strlen(msg));


#if START_OS_DEMO
/**/
xTaskCreate( vLEDTask, ( const char * const ) "LedTask", configMINIMAL_STACK_SIZE, (void*)4, mainLED_TASK_PRIORITY, NULL );
xTaskCreate( vLEDTask, ( const char * const ) "LedTask", configMINIMAL_STACK_SIZE, (void*)1, mainLED_TASK_PRIORITY+1, NULL );
xTaskCreate( vLEDTask, ( const char * const ) "LedTask", configMINIMAL_STACK_SIZE, (void*)2, mainLED_TASK_PRIORITY+2, NULL );
xTaskCreate( vLEDTask, ( const char * const ) "LedTask", configMINIMAL_STACK_SIZE, (void*)3, mainLED_TASK_PRIORITY+3, NULL );

xTaskCreate( uartTask, ( const char * const ) "UARTTask", configMINIMAL_STACK_SIZE, (void*)0, mainLED_TASK_PRIORITY+4, NULL );

//ptr to entry fn(name of fn),descriptive name of task(debugger),no of words, value passed to create task, priority, optional
/* Start the scheduler. */
vTaskStartScheduler();
#endif

 

Krishnaja.

タグ(1)
0 件の賞賛
返信

4,728件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

could you send me whole project? I'm afraid the main is not enough in this case.

Thanks,

Lukas

 

0 件の賞賛
返信

4,707件の閲覧回数
Krishnaja
Contributor II

Hi,

PFA

 

Regards,

Krishnaja.

0 件の賞賛
返信

4,690件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

It is mandatory to call init and other functions (if drivers uses OS services) after starting scheduler. Otherwise it won't work.

Regards,

Lukas

 

 

0 件の賞賛
返信

4,672件の閲覧回数
Krishnaja
Contributor II

Hi,

Tell me how to call init and what other functions should i call and where?

 

Krishnaja.

0 件の賞賛
返信

4,645件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport
0 件の賞賛
返信