How to Use User Switch on DEVKIT-MPC5748G?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

How to Use User Switch on DEVKIT-MPC5748G?

3,759件の閲覧回数
Elsa_24
Contributor II
Hi, I am trying to familiarize myself with the DEVKIT-MPC5748G. So far I have been able to turn on a user LED. Now I want to control the LED (on and off) with a user switch. I have activated for example the PORT PA3 connected to the User Switch4 as input already. But how do I set the condition "If User Switch4 is pressed then the LED lights up and otherwise the LED stays off"?) Thanks
0 件の賞賛
返信
7 返答(返信)

3,634件の閲覧回数
polisetty
Contributor II

Hi I am trying to write a program  to control the LED (on and off) with a user switch. If I press the switch the LED must ON and otherwise it remains OFF.(by using MPC5748G controller)

can any one tell me how to write program for that ? 

0 件の賞賛
返信

3,595件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

I guessed this was discussed in this thread.
For example add below code to the simple "hello_Z4_1" example

SIUL2.MSCR[PA10].B.OBE = 1; /* Pad PA10 (10): OBE=1. On EVB active low DS4 LED */
SIUL2.MSCR[PA3].B.IBE = 1; /* Pad PA3 (3): IBE=1. On EVB switch SW4 */

while(1)
{
     if(SIUL2.GPDI[PA3].R) // PA3 high / SW4 pressed
    {
       SIUL2.GPDO[PA10].R = 0;//LED ON
    }
    else //PA3 low / SW4 released
    {
       SIUL2.GPDO[PA10].R = 1;//LED OFF
    }
}

BR, Petr

0 件の賞賛
返信

3,753件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

if(SIUL2.GPDI[3].R) // PA3 high / SW4 pressed
{
   //LED ON
}
else   /PA3 low / SW4 released
{

   //LED OFF
}

BR, Petr

3,747件の閲覧回数
Elsa_24
Contributor II

Hi PetrS,

Thanks for your answer.

I tried to do as you suggested but I got an error in the if condition:

<<request for member 'GPDI' in something not a structure or union>>

how to solve the problem?

Here is the corresponding part of my code. The erector signals at the level of the condition in the if

if(SIUL2.GPDI[3].R)
{
PINS_DRV_WritePin(PTA, 10, 1);
}
else
{
PINS_DRV_WritePin(PTA, 10, 0);

}

 

PS: I have activated PORT PA3 in SIUL2 as an input already. it corresponds to GPIO 3

0 件の賞賛
返信

3,741件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

check how registers are defined in the device header file.
Under SDK you can use PINS_DRV_ReadPins function.

The usage should be
pin_value = ((uint16_t)(1<<(pin))&PINS_DRV_ReadPins(port))>>(pin);

In your code you can can have e.g.

if((uint16_t)(1<<(3))&PINS_DRV_ReadPins(PTA))
{
     PINS_DRV_WritePin(PTA, 10, 1);
}
else
{
     PINS_DRV_WritePin(PTA, 10, 0);
}

BR, Petr

0 件の賞賛
返信

3,706件の閲覧回数
Krishnaja
Contributor II

Hi @PetrS ,

I am  also getting same error in if loop. "Request for member 'GPDI' in something not a structure or union", I have enclosed the project. 

Please tell me how to resolve the error.

Thanks

Krishnaja.

0 件の賞賛
返信

3,685件の閲覧回数
PetrS
NXP TechSupport
NXP TechSupport

Hi,

did you read my latest post? 
Either use driver function
if((uint16_t)(1<<(3))&PINS_DRV_ReadPins(PTA))
or according header file use 
if(SIUL2->GPDI[3])

BR, Petr

0 件の賞賛
返信