FlexRay on MPC5748G - Basics implementation

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FlexRay on MPC5748G - Basics implementation

1,914 Views
bassduty
Contributor II

Hello,

I'm trying to write a very basic FlexRay Test code, actually for the moment just to test hardware. There is no OS.

I have some questions about basic stuff :

  1. how can I determine the System Memory Base Address Register (FR_SYMBADR). I mean how to "choose" this address and assure that there is not conflict with other part of code. Because this choosen address will be in a register but not "reserved" by the code. Is it absolutely mandatory to map this address with a structure ?
  2. I understand that the data field part of physical message buffer is linked to the header part via the data field offset (FR_MBDOR). But these data field offset has to be calculated by the application in order to fill FR_MBDOR. Actually, based on the reference manual reading I don't understand how to calculate them. Could you give a example with 2 messages buffers ?
  3. I don't understand the purpose of the message buffer segment feature ( FR_MBDSR[MBSEG1DS]  and FR_MBDSR[MBSEG2DS]).
    I'm beginner with FlexRay. This is the reason of so basics questions.

Thanks in advance.

Regards

Tags (2)
0 Kudos
Reply
1 Reply

1,460 Views
1134025279
Contributor I

Hi,Jonathan

I have the same question as you.

Did you solve the problem? Could you please share us your solution?

Thanks a lot!

0 Kudos
Reply