Finding Flash Module which cause ECC

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Finding Flash Module which cause ECC

ソリューションへジャンプ
1,985件の閲覧回数
20Sidar04
Contributor III

Dear Mr. / Mrs.,

When check sample code named MPC5777C-1b+2b_FLASH_ECC_error_injection, software delete content of FLASH for solve ECC error. Without it, does it available solve ECC error without deleting? I wonder that. My source could find FLASH module which cause ECC error? In IVOR exception, I wanna find reason FLASH module number which cause this error. 

Best Regards.

タグ(3)
0 件の賞賛
返信
1 解決策
1,974件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hello,

Without it, does it available solve ECC error without deleting?

It depends, multibit error is not possible to repair and erase is needed in order to get flash in correct state.

In case of single bit error, the device will auto correct it and you will read correct data. But the ECC single bit error will stay in physical memory until you erase it.

My source could find FLASH module which cause ECC error?

Sure, you can read address where the ECC fault is and also type of ECC fault inb FCCU module.

Have a closer look at this document, where all is described in details:

https://www.nxp.com/docs/en/application-note/AN5200.pdf

Best regards,

Peter

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,975件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hello,

Without it, does it available solve ECC error without deleting?

It depends, multibit error is not possible to repair and erase is needed in order to get flash in correct state.

In case of single bit error, the device will auto correct it and you will read correct data. But the ECC single bit error will stay in physical memory until you erase it.

My source could find FLASH module which cause ECC error?

Sure, you can read address where the ECC fault is and also type of ECC fault inb FCCU module.

Have a closer look at this document, where all is described in details:

https://www.nxp.com/docs/en/application-note/AN5200.pdf

Best regards,

Peter

0 件の賞賛
返信