FNET stack for MPC5777c with s32 iDE for power Architecture 2017_R1

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FNET stack for MPC5777c with s32 iDE for power Architecture 2017_R1

2,156 Views
vignesh_v
Contributor III

Hi, 

    I need to develop a TFTP using FEC of MPC5777c. Request to help me with FNET stack for using the socket and other needs. for MPC5777c and s32 iDE for power Architecture 2017_R1 IDE

Labels (1)
0 Kudos
Reply
6 Replies

2,010 Views
vignesh_v
Contributor III

Can the stack be used to port the same for MPC5777C for file transfer using TFTP thro ethernet port?

Regards,

Vignesh.V

0 Kudos
Reply

2,010 Views
martin_kovar
NXP Employee
NXP Employee

Hello Vignesh,

yes, FNET stack supports TFTP service.

Regards,

Martin

0 Kudos
Reply

2,010 Views
vignesh_v
Contributor III

Thanks Martin,

                       I looked at the example given for MPC5774P. If i need to use the stack for MPC5777C which files needs to be changed specifically for MPC5777C? or the same stack can be used unchanged? 

0 Kudos
Reply

2,010 Views
PetrS
NXP TechSupport
NXP TechSupport

you should modify/add files in mpc directory.

It should be in ../fnet_stack/port/cpu/mpc/

In MPC5744P example it is fnet_stack/cpu/mpc/

BR, Petr

0 Kudos
Reply

2,010 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

as far as I know we do not have FNET port for MPC5777C, however there exist customer MPC5744P port which you can refer to, see MPC5744P FNET S32DS 

Or you can get some tips directly on FNET user forum;https://sourceforge.net/p/fnet/discussion/920346/ 

BR, Petr

0 Kudos
Reply

2,010 Views
vignesh_v
Contributor III

Thanks. Can the stack be used to port the same for MPC5777C for file transfer using TFTP thro ethernet port?

Regards,

Vignesh.V

0 Kudos
Reply