FLASH B erase error MPC5676

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

FLASH B erase error MPC5676

跳至解决方案
3,899 次查看
CCandido
Contributor V

hi,

I have problems with Erase block B flash MPC5676.

Block A erase ok, L0~L9, M1~M0 and L0/M0 <   update help

flash_b.png

//----------------code test FLASH_B

DCACHE_Disable();  withh/winout

FLASH_B.HLR.R = 0xB2B22222; //password
FLASH_B.HLR.B.HBLOCK = 0x00 ; //unlock all blocks in high address space
//Erase
FLASH_B.MCR.B.ERS = 1;
FLASH_B.HSR.B.HBSEL = 0x01;  //  blocks H0 
*(unsigned int *) 0x100000 = 0xFFFFFFFF;

FLASH_B.MCR.B.EHV = 1;
while ((FLASH_B.MCR.B.DONE == 0));
FLASH_B.MCR.B.EHV = 0;
FLASH_B.MCR.B.ERS = 0;
peg = FLASH_A.MCR.B.PEG;

//-------------------------updating it help

thanks,

Carlos.

标签 (1)
标记 (1)
0 项奖励
回复
1 解答
3,668 次查看
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi Carlos,

the flash is interleaved in high address space:

pastedImage_1.png

This helps to improve the performance. In case of non-interleaved flash, two physical reads of flash arrays are needed to fill one cache line. If the flash is interleaved, the blocks are read in parallel, so it looks like only one physical read is necessary.

The interlock write to 0x10_0000 falls to flash block A. So, it does not work as you can see. You need to write to 0x10_0000+16.

Or you can use SSD flash drivers which handle everything on background and you use the flash as linear address space. You do not need to care about blocks A and B ever:

https://www.nxp.com/lgfiles/Qorivva/MPC5674F_C90FL_SSD_DRV.exe 

Regards,

Lukas

在原帖中查看解决方案

0 项奖励
回复
4 回复数
3,669 次查看
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi Carlos,

the flash is interleaved in high address space:

pastedImage_1.png

This helps to improve the performance. In case of non-interleaved flash, two physical reads of flash arrays are needed to fill one cache line. If the flash is interleaved, the blocks are read in parallel, so it looks like only one physical read is necessary.

The interlock write to 0x10_0000 falls to flash block A. So, it does not work as you can see. You need to write to 0x10_0000+16.

Or you can use SSD flash drivers which handle everything on background and you use the flash as linear address space. You do not need to care about blocks A and B ever:

https://www.nxp.com/lgfiles/Qorivva/MPC5674F_C90FL_SSD_DRV.exe 

Regards,

Lukas

0 项奖励
回复
3,668 次查看
CCandido
Contributor V

hi Lukas,

my code in RAM without ISR and exceptions_table,

so I chose the way to work with interlock.

write flash control address no problem, no near code have,

 Erase high-address all space.

have solution do withot SSD driver ?

my test SSD   : VLE_ON, COPYRAM_FALSE

ret = pFlashInit( &ssdConfig );  call not  return

thanks,

Carlos

0 项奖励
回复
3,668 次查看
lukaszadrapa
NXP TechSupport
NXP TechSupport

As I mentioned, there's no problem with your code. The interlock write just must fall within block B, that means you need to write to 0x10_0010, not to 0x10_0000.

Regarding SSD driver - I would need to see your code.

Regards,

Lukas

0 项奖励
回复
3,668 次查看
CCandido
Contributor V

hi Lukas,

SSD solved problems,

thanks,

Carlos.

0 项奖励
回复