Example SBC nxp5744p Repo not found

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Example SBC nxp5744p Repo not found

5,666 Views
rehab_hassan
Contributor II

I installed S32 design studio and the update package, open sbc example 

I have this error 

rehab_hassan_0-1678475793613.png

 

0 Kudos
Reply
13 Replies

5,624 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

I am just checking my installation: v2.1 with SDK3.0.3. and I see the PA_15 is there.

petervlna_0-1678781482357.pngpetervlna_1-1678781598336.png

Then the project is loaded form example and I can compile it.

Are you even able to create it?

Best regards,

Peter

 

0 Kudos
Reply

5,617 Views
rehab_hassan
Contributor II

This window doesn't pop up with me, 

If I pressed the continue loading, the following appear with me:

rehab_hassan_0-1678782464466.png

 

rehab_hassan_1-1678782490598.png

 

 

 

0 Kudos
Reply

5,639 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

Since you are not sharing much information here could you please do so?

Which version of S32DS are you using, drivers, etc...?

Best regards,

Peter

 

0 Kudos
Reply

5,633 Views
rehab_hassan
Contributor II

I installed S32 design studio for power architecture Version 2.1

and installed this updates 

rehab_hassan_0-1678725604687.png

should I install anything else?

0 Kudos
Reply

5,596 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

this is correct configuration. If you still get the same error if you Create new project from Example:

jiri_kral_0-1678876211165.png

 

please try to uninstall and install again SDK v3.0.3. The installation may be corrupted. 

jiri_kral_1-1678876299606.png

 

 

0 Kudos
Reply

5,593 Views
rehab_hassan
Contributor II

I tried to reinstall it multiple times and with different laptops and I have the same issue all the time

0 Kudos
Reply

5,591 Views
jiri_kral
NXP Employee
NXP Employee

Hi, 

did you tried start with the new workspace? If not, this may also solve your issue. If it doesn't help, please share the log file from your workspace. The file is in workspace_folder/.metadata 

0 Kudos
Reply

5,589 Views
rehab_hassan
Contributor II

Kindly find attached metadata

0 Kudos
Reply

5,527 Views
rehab_hassan
Contributor II

I shared log and the whole folder ./metadata 

any advice?

0 Kudos
Reply

5,489 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

Please have a look at this thread.

There is one solution for this issue, which could help you.

https://community.nxp.com/t5/MPC5xxx/I-get-the-following-error-when-i-laund-the-S32-IDE/m-p/1616682#...

best regards,

Peter

0 Kudos
Reply

5,640 Views
rehab_hassan
Contributor II

 

rehab_hassan_1-1678697295517.png

 

 

rehab_hassan_0-1678697246109.png

 

 

0 Kudos
Reply

5,642 Views
rehab_hassan
Contributor II

yes this solution doesn't work with me

0 Kudos
Reply

5,644 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

Please have a look at following thread:

https://community.nxp.com/t5/MPC5xxx/Where-can-download-the-quot-SDK-S32-PA-15-quot-for-MPC5744P/m-p...

Best regards,

Peter

0 Kudos
Reply