Example SBC nxp5744p Repo not found

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Example SBC nxp5744p Repo not found

5,732 次查看
rehab_hassan
Contributor II

I installed S32 design studio and the update package, open sbc example 

I have this error 

rehab_hassan_0-1678475793613.png

 

0 项奖励
回复
13 回复数

5,690 次查看
petervlna
NXP TechSupport
NXP TechSupport

Hello,

I am just checking my installation: v2.1 with SDK3.0.3. and I see the PA_15 is there.

petervlna_0-1678781482357.pngpetervlna_1-1678781598336.png

Then the project is loaded form example and I can compile it.

Are you even able to create it?

Best regards,

Peter

 

0 项奖励
回复

5,683 次查看
rehab_hassan
Contributor II

This window doesn't pop up with me, 

If I pressed the continue loading, the following appear with me:

rehab_hassan_0-1678782464466.png

 

rehab_hassan_1-1678782490598.png

 

 

 

0 项奖励
回复

5,705 次查看
petervlna
NXP TechSupport
NXP TechSupport

Hello,

Since you are not sharing much information here could you please do so?

Which version of S32DS are you using, drivers, etc...?

Best regards,

Peter

 

0 项奖励
回复

5,699 次查看
rehab_hassan
Contributor II

I installed S32 design studio for power architecture Version 2.1

and installed this updates 

rehab_hassan_0-1678725604687.png

should I install anything else?

0 项奖励
回复

5,662 次查看
jiri_kral
NXP Employee
NXP Employee

Hi, 

this is correct configuration. If you still get the same error if you Create new project from Example:

jiri_kral_0-1678876211165.png

 

please try to uninstall and install again SDK v3.0.3. The installation may be corrupted. 

jiri_kral_1-1678876299606.png

 

 

0 项奖励
回复

5,659 次查看
rehab_hassan
Contributor II

I tried to reinstall it multiple times and with different laptops and I have the same issue all the time

0 项奖励
回复

5,657 次查看
jiri_kral
NXP Employee
NXP Employee

Hi, 

did you tried start with the new workspace? If not, this may also solve your issue. If it doesn't help, please share the log file from your workspace. The file is in workspace_folder/.metadata 

0 项奖励
回复

5,655 次查看
rehab_hassan
Contributor II

Kindly find attached metadata

0 项奖励
回复

5,593 次查看
rehab_hassan
Contributor II

I shared log and the whole folder ./metadata 

any advice?

0 项奖励
回复

5,555 次查看
petervlna
NXP TechSupport
NXP TechSupport

Hello,

Please have a look at this thread.

There is one solution for this issue, which could help you.

https://community.nxp.com/t5/MPC5xxx/I-get-the-following-error-when-i-laund-the-S32-IDE/m-p/1616682#...

best regards,

Peter

0 项奖励
回复

5,706 次查看
rehab_hassan
Contributor II

 

rehab_hassan_1-1678697295517.png

 

 

rehab_hassan_0-1678697246109.png

 

 

0 项奖励
回复

5,708 次查看
rehab_hassan
Contributor II

yes this solution doesn't work with me

0 项奖励
回复

5,710 次查看
petervlna
NXP TechSupport
NXP TechSupport

Hello,

Please have a look at following thread:

https://community.nxp.com/t5/MPC5xxx/Where-can-download-the-quot-SDK-S32-PA-15-quot-for-MPC5744P/m-p...

Best regards,

Peter

0 项奖励
回复