Enabling HSE bit via DCF record

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Enabling HSE bit via DCF record

1,353件の閲覧回数
ayeshap
Contributor I

Hi petervlna,

I'm working on MPC5748G micro. I want to know that where does NXP write DCF record to enable HSM i.e, to set HSE bit of SSCM_UOPS register ?

In boards where HSM is not enable, we enable it by flashing .cmm file (SHE firmware RTM1.0.5) which has a particular DCF  record to be written in UTEST area.

 

What about boards which are HSM enabled by NXP itself ? Where is that DCF record written or there is other way to enable HSE bit?

 

Awaiting response at your earliest convenience .

Regards,

Ayesha

0 件の賞賛
返信
1 返信

1,316件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hello,

I'm working on MPC5748G micro. I want to know that where does NXP write DCF record to enable HSM i.e, to set HSE bit of SSCM_UOPS register ?

On samples containing HSM firmware we do it in NXP fab by writing to UTEST the DCF record. This process can be done only once. If you want to enable it you can do it according the HSM security reference manual appending A.

What about boards which are HSM enabled by NXP itself ? Where is that DCF record written or there is other way to enable HSE bit?

The record is written in UTEST flash. Once it is enabled (by NXP or user) it is permanent.

regards,

Peter

0 件の賞賛
返信