MPC5748G gets two ez200z4 cores and one ez200z2 core, I need to know the DMIPS of MPC5748G to evaluate the performance of MPC5748G, could you help me with this question?
Hi, we usually don’t provide MIPS values for MPC5xxx as it does not make too much sense because these MCUs are being selected according different criteria (presence of certain special modules as so on..) but I have found some approximate numbers for the cores used with mentioned MCUs (checker cores omitted)
MPC5748G – 2 x e200z420 + 1x e200z210
e200z420 - 2.381 (DMips/MHz)
Unfortunately I haven’t found numbers for e200z210, but it is similar core as e200z420 without data/instruction caches, running at half frequency.
Please take these number only as indicative as it depends on lot of factors (memories, caches, optimizations, application itself and so on.)