EEPROM

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

EEPROM

6,227 次查看
emerging
Contributor III

Hello engineers,

I am using MPC5746 micro controller.I need to write one 32 bit variable in to eeprom through my program.I know its memory location,and its 0x00800000 to 0x00803FFF. Any one can tell me how to write to this memory location in eeprom.Any one can share an example code. Please give your valuable comments...Thank you

标记 (1)
8 回复数

5,202 次查看
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

there are three options:

1. Use SSD flash driver:

http://www.nxp.com/assets/downloads/data/en/device-drivers/C55_JDP_SSD.exe 

User manual and examples are included in the package.

I shared simple example using SSD flash drivers here:

Example MPC5748G Flash RW SSD 

2. Use EEPROM Emulation driver:

http://www.nxp.com/assets/downloads/data/en/device-drivers/MPC5xxx_EEE_DRIVER.exe 

3. And the last option - write own functions for flash programming. I shared simple example here (it's the same example like above, just without the drivers):

https://community.nxp.com/docs/DOC-105380 

Regards,

Lukas

5,202 次查看
hc17
Contributor I

Hello, Lukas,

I'm using EEPROM Emulation on MPC5744P. Now I have met a problem.

Before eeprom initialization, I have a program with run time 5ms, but after initialization, I need 14ms-15ms to finish the program. Have you ever met these kind of problems? Could you please give me some suggestions to solve this problem?

Thank you.

This picture is before initialization

pastedImage_2.png

This picture is after initialization

pastedImage_1.png

0 项奖励
回复

5,202 次查看
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

it's not clear to me. Do you mean that init_eeprom adds significant delay? You can check the source code, there may be a lot of things to be done. Or do you mean that the execution time of other functions gets longer? In this case, it would require more debugging to find what takes more time. One option is to toggle a pin at beginning and at end of each function (you can use different pins) and check them by scope to find the root cause.

Regards,

Lukas

0 项奖励
回复

5,202 次查看
emerging
Contributor III

 Thank you Lukas, I think its better to use 3rd option.Thanks for your support. i have one more doubt can we write a variable to an uninitialized memory directly by using its address using pointer?

eg : int*nb=(int*)0x00800000;

       *nb=a0;

here the value in variable a0 will write to address 0x00800000 or not?

0 项奖励
回复

5,202 次查看
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

you need to follow the sequence described in reference manual. This is procedure for program operation:

pastedImage_1.png.

And this is implementation of the procedure in my SW example which I shared earlier:

    //program one page in the mid block
    C55FMC.MCR.B.PGM = 1;
    *(unsigned int*)0x00FB8000 = 0x11111111;    //interlock write
    *(unsigned int*)0x00FB8004 = 0x22222222;    //up to 8 words (one 256bit page) can be programmed at once
    *(unsigned int*)0x00FB8008 = 0x33333333;
    *(unsigned int*)0x00FB800C = 0x44444444;
    *(unsigned int*)0x00FB8010 = 0x55555555;
    *(unsigned int*)0x00FB8014 = 0x66666666;
    *(unsigned int*)0x00FB8018 = 0x77777777;
    *(unsigned int*)0x00FB801C = 0x88888888;
    C55FMC.MCR.B.EHV = 1;
    while(C55FMC.MCR.B.DONE == 0);
    C55FMC.MCR.B.EHV = 0;
    C55FMC.MCR.B.PGM = 0;

Regards,

Lukas

5,202 次查看
emerging
Contributor III

 Thanks you Lukas.I read it and now more clear,Please find the following modified code :

 I am going to write 3 values that are saved in 3 globally declared 32 bit variables uint32_t a0,a1,a2 ;

    C55FMC.MCR.B.PGM = 1;

    unsigned int *nb=(unsigned int*)0x00800000;

    *nb=a0;

     nb++;

    *nb=a1;

     nb++;

    *nb=a2;
    C55FMC.MCR.B.EHV = 1;
    while(C55FMC.MCR.B.DONE == 0);
    C55FMC.MCR.B.EHV = 0;
    C55FMC.MCR.B.PGM = 0;

0 项奖励
回复

5,202 次查看
lukaszadrapa
NXP TechSupport
NXP TechSupport

No problem here. Just be aware that these two double words must be in erased state because cumulative programming is not allowed. If these two double words are not erased, it is necessary to erase whole 16KB block.

Regards,

Lukas

0 项奖励
回复

5,202 次查看
burnyfu
Contributor II

Hi Lukas,

I am using MPC5744 micro controller.I can successfully write data at 0x800000 addresses,but when I restart the power after reading out the data 0xFF. I was debugging in the S32DS to determine the success of the write.

The code is as follows:

C55FMC.MCR.B.PGM = 1;
*(uint8*)(0x800000) = 0x11;
C55FMC.MCR.B.EHV = 1;
while(C55FMC.MCR.B.DONE == 0);
C55FMC.MCR.B.PEG = 1;
C55FMC.MCR.B.EHV = 0;
C55FMC.MCR.B.PGM = 0;

0 项奖励
回复