Dual Core enabling In MPC5775B

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Dual Core enabling In MPC5775B

1,455 Views
NarsimhaKorra
Contributor I

Hii all,
Here are the things what I have done!
Just created multi-core independent projects for MPC5775B in S32DS IDE for two LEDs blinking in two cores. But core0 is getting enabled after flashing the code but not core1 and core1 is getting stated after the manual reset is done or after a power cycle .


Can any one help how to enable core1 along with core0 at time without doing the manual reset.

0 Kudos
Reply
2 Replies

1,437 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

Hard to say.  Usually the reset is done by SIU from the uC on core enable event.

petervlna_0-1743746951620.pngpetervlna_0-1743746951620.png

 

Have a look at reference example:

https://community.nxp.com/docs/DOC-335462

 

Best regards,

Peter

0 Kudos
Reply

1,255 Views
NarsimhaKorra
Contributor I

We have tried with the SIU->RSTVEC1 register, but still it's not working. Need a solution for this. I have attached the project zip here. Please look into it and suggest the required changes.

0 Kudos
Reply