DSPI

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 
4,425 Views
zhhq123
Contributor II

How to send 32-bit data when DSPI is in master mode?Are there any example code or configuration advice?(I want to use MPC5634 to drive TLE82453)

0 Kudos
Reply
1 Solution
4,414 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

Use two 16-bit frames. First PUSH command will be configured with CONT=1, second with CONT=0. This way CS stays asserted between 16-bit frames and it acts as one 32-bit data frame.

I can offer you an example code showing SPI communication with external flash memory S25FL129P. Used device was MPC5676R that is MCU similar to MPC5634M having compatible DSPI module:

https://community.nxp.com/docs/DOC-335461

View solution in original post

0 Kudos
Reply
4 Replies
4,415 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

Use two 16-bit frames. First PUSH command will be configured with CONT=1, second with CONT=0. This way CS stays asserted between 16-bit frames and it acts as one 32-bit data frame.

I can offer you an example code showing SPI communication with external flash memory S25FL129P. Used device was MPC5676R that is MCU similar to MPC5634M having compatible DSPI module:

https://community.nxp.com/docs/DOC-335461

0 Kudos
Reply
4,364 Views
zhhq123
Contributor II

Hi, davidtosenovjan:

       I refer to your advice to config DSPI(CONT = 1).Now,

the PCS signal remains asserted for the duration of the two transfers.

;But SCK signal inserted Tcsc and Tasc.

微信图片_20210108214055.jpg微信图片_20210108214107.jpg

 

 

 

 

 

 

 

 

0 Kudos
Reply
4,381 Views
zhhq123
Contributor II

Hi davidtosenovjan:

        I refer to the example you provided to write the following code,but it didn't work.I have no idea to modify.Are there any advice you can provided.

 

void initDSPI_B(void) {
DSPI_B.MCR.R = 0x80010001; /* Configure DSPI_B as Master */
DSPI_B.CTAR[0].R = 0x700C0021; /* Configure CTAR0 */
DSPI_B.MCR.B.HALT = 0x0; /* Exit HALT mode: go from STOPPED to RUNNING state*/

SIU.PCR[102].R = 0x060C; /* MPC555x: Config pad as DSPI_B SCK Output */
SIU.PCR[103].R = 0x050C; /* MPC555x: Config pad as DSPI_B SIN input */
SIU.PCR[104].R = 0x060C; /* MPC555x: Config pad as DSPI_B SOUT output*/
SIU.PCR[105].R = 0x060C; /* MPC555x: Config pad as GPIO high output SPI_CS */

SIU.PCR[109].R = 0x0300; /* MPC555x: Config pad as GPIO high output RESET_MCU*/
SIU.PCR[106].R = 0x0300; /* MPC555x: Config pad as GPIO high output ENABLE_MCU*/
SIU.PCR[110].R = 0x0100; /* MPC555x: Config pad as GPIO Input FAULT_MCU*/

SIU.GPDO[106].B.PDO = 1;
SIU.GPDO[109].B.PDO = 1;

}

 

 

int main(void)
{
initSysclk();
initDSPI_B();
xcptn_xmpl (); /* Configure and Enable Interrupts */
CAN_A_init();
init_PIT_RTI();


DSPI_B.SR.R= 0x10000000;
DSPI_B.PUSHR.R = 0x80018300;//78020000;
while(!(DSPI_B.SR.B.RFDF)){}
dummy_var = (uint8_t)(DSPI_B.POPR.R);
DSPI_B.SR.R = 0x80020000;
DSPI_B.PUSHR.R = 0x08011040;
while(!(DSPI_B.SR.B.RFDF)){}
dummy_var = (uint8_t)(DSPI_B.POPR.R);
DSPI_B.SR.R = 0x80020000;


DSPI_B.PUSHR.R = 0x8001A860; 
while(!(DSPI_B.SR.B.RFDF)){}
dummy_var = (uint8_t)(DSPI_B.POPR.R);
DSPI_B.PUSHR.R = 0x080100FA; //1KHz
while(!(DSPI_B.SR.B.RFDF)){}
dummy_var = (uint8_t)(DSPI_B.POPR.R);
DSPI_B.SR.R = 0x80020000;


DSPI_B.PUSHR.R = 0x80009080; //setpoint
while(!(DSPI_B.SR.B.RFDF)){}
dummy_var = (uint8_t)(DSPI_B.POPR.R);
DSPI_B.PUSHR.R = 0x080003FF;
while(!(DSPI_B.SR.B.RFDF)){}
dummy_var = (uint8_t)(DSPI_B.POPR.R);
DSPI_B.SR.R = 0x80020000;
/* Loop forever */
for(;;)
{
}
}

 

       

0 Kudos
Reply
4,407 Views
zhhq123
Contributor II

Okay,Thanks for your reply

0 Kudos
Reply