DSPI Interrupt Request and Enable Register

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DSPI Interrupt Request and Enable Register

1,513 Views
alexrebega
Contributor I

Hi

Why does the reference manual of MPC5607B state that one should not write into DSPIx_RSER while the DSPI is running. If I want to disable one interrupt, why should I halt the entire module at first and not disable it by directly writing in RSER?

Thank you.

Labels (1)
Tags (2)
0 Kudos
Reply
1 Reply

1,393 Views
PetrS
NXP TechSupport
NXP TechSupport

Hi,

Writing to the DSPIx_RSER should not be done while DSPI is running to avoid losing of ISR or DMA request, I think.

If DSPI is in running state you should not write to any configuration register, also to DSPIx_RSER.

When DSPI is in stopped state there should be no issue to modify it. The TXRXS bit in the DSPIx_SR can be used to determine the DSPI state.

BR, Petr

0 Kudos
Reply