DEVKIT-MPC5748G MCAL example error

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

DEVKIT-MPC5748G MCAL example error

1,074件の閲覧回数
canegatto
Contributor I

I tried to build and flash the MPC574XG_MCAL4_0_RTM_1_0_5_Sample_Application provided in MCAL package by NXP. The project build succesfully with Windriver compiler, but after the flashing (done with the run.cmm Lauterbach script) the CPU after a few steps stops at IVOR1_Handler ( # IVOR1 - 0x1010 - Machine Check Interrupt (SPR 401) ). 

Being the default example, I would expect the board to run the default flashed application, but it seems stuck instead. What are the possible causes of the problem? 

0 件の賞賛
返信
1 返信

928件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hi,

What is the instruction that caused IVOR1?

Could you share more information on this? Some debugging screens where we can see the issue?

Also compiled code could help. I can run it here and see where it fails.

regards,

Peter

0 件の賞賛
返信