DEVKIT-MPC5748G MCAL example error

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

DEVKIT-MPC5748G MCAL example error

1,063 Views
canegatto
Contributor I

I tried to build and flash the MPC574XG_MCAL4_0_RTM_1_0_5_Sample_Application provided in MCAL package by NXP. The project build succesfully with Windriver compiler, but after the flashing (done with the run.cmm Lauterbach script) the CPU after a few steps stops at IVOR1_Handler ( # IVOR1 - 0x1010 - Machine Check Interrupt (SPR 401) ). 

Being the default example, I would expect the board to run the default flashed application, but it seems stuck instead. What are the possible causes of the problem? 

0 Kudos
Reply
1 Reply

917 Views
petervlna
NXP TechSupport
NXP TechSupport

Hi,

What is the instruction that caused IVOR1?

Could you share more information on this? Some debugging screens where we can see the issue?

Also compiled code could help. I can run it here and see where it fails.

regards,

Peter

0 Kudos
Reply