D_CLKOUT Frequency Tolerance MPC5674F

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

D_CLKOUT Frequency Tolerance MPC5674F

Jump to solution
2,829 Views
CNarendra
Contributor III

Hi,

Could you please confirm the frequency tolerance of the EBI D_CLKOUT signal on the MPC5674F? We couldn't find this detail in the datasheet or reference manual.

Thanks,
Narendra C

MPC5674F ,#EBI 

Tags (1)
0 Kudos
Reply
1 Solution
2,753 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

You can consider it as PLL contribution (worst case) to XOSC tolerance.

View solution in original post

0 Kudos
Reply
5 Replies
2,804 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

The D_CLKOUT signal is derived from the system clock via the FMPLL.
While the nominal frequency of D_CLKOUT can be configured, the tolerance depends on the accuracy of the external oscillator used as the PLL reference.

0 Kudos
Reply
2,800 Views
CNarendra
Contributor III

Hi @davidtosenovjan ,

Is there any frequency tolerance introduced by the microcontroller itself, aside from the external crystal?

- Narendra.C

0 Kudos
Reply
2,791 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

Actually DS specifies directly CLKOUT jitter:

davidtosenovjan_0-1748007310344.png

 

0 Kudos
Reply
2,761 Views
CNarendra
Contributor III


Whether CLKOUT jitter value can be considered as FCLKOUT tolerance?

-Narendra 

0 Kudos
Reply
2,754 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

You can consider it as PLL contribution (worst case) to XOSC tolerance.

0 Kudos
Reply