Crash when debugging with iSystem BlueBox and enabling MSR.ME

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Crash when debugging with iSystem BlueBox and enabling MSR.ME

Jump to solution
1,255 Views
mikel1
Contributor II

Hi,

I'm trying to debug a program for a MPC5744P using iSystem's Bluebox and winIDEA. However it seems to crash when it is executing the initialization dissassembly code. Specifically, it seems to crash when it enables the MSR.ME bit:

;#*************************** Enable ME Bit in MSR *****************************
    mfmsr    r6
    e_or2i   r6, 0x1000
    mtmsr    r6

This bit seems to be used to enable Asynchronous Machine Check interrupts. The moment I run this section the program simply jumps to addess 0x0000 0010. I don't know why this happens.

I can skip the execution of this whole section, but I believe this might be causing some other problems with the code I'm trying to debug.

Anyone has had a similar problem before?

0 Kudos
Reply
1 Solution
1,246 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

Yes, ME enable machine check interrupts.

So I expect that you have already active and pending machine check interrupt and once you enable ME, it is immediately processed and executed.

Since it is jumping to address 0x10 and there it crash, I expect you do not have any handlers for IVOR1 vector in your code.

Have a look at 15.8 Exceptions chapter of reference manual.

Best regards,

Peter

View solution in original post

0 Kudos
Reply
2 Replies
1,240 Views
mikel1
Contributor II

Hi,

Thanks for the answer. You were right. There was an exception in the code, and it seems it was still pending even after I reflashed the program. So when the program enabled MSR.ME it it jumped to the address 0x10.

0 Kudos
Reply
1,247 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

Yes, ME enable machine check interrupts.

So I expect that you have already active and pending machine check interrupt and once you enable ME, it is immediately processed and executed.

Since it is jumping to address 0x10 and there it crash, I expect you do not have any handlers for IVOR1 vector in your code.

Have a look at 15.8 Exceptions chapter of reference manual.

Best regards,

Peter

0 Kudos
Reply