Could'nt enter IVOR6 Exception Handler

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Could'nt enter IVOR6 Exception Handler

ソリューションへジャンプ
2,736件の閲覧回数
20Sidar04
Contributor III

Dear Mr. / Mrs.

I try to cause illegal instruction exception by following source code on MPC5777C;

typedef void (*myfunc)();
myfunc foo = 0;
foo();

This shows that I am on right way.

20Sidar04_0-1645458429921.png

As I see, when I tried debug my controller. My program is not stop on IVOR6_Exception_Handler. 

How to handle this problem. I tried to cause IVOR6 exception for MPC5777C.

Best regards.

 

タグ(3)
0 件の賞賛
返信
1 解決策
2,726件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

se_illegal instruction (opcode 0x0000) then it depends if the device is running in debug mode or in standalone mode:

- in debug mode, se_illegal works like software breakpoint. IVOR6 is not triggered. If you just step the code, it works like nop instruction. If you run the code and the program reaches se_illegal instruction, the device will stop execution and it will enter debug mode.

- if the device is running in standalone without debugger, se_illegal will trigger IVOR6 exception.

元の投稿で解決策を見る

0 件の賞賛
返信
2 返答(返信)
2,727件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

se_illegal instruction (opcode 0x0000) then it depends if the device is running in debug mode or in standalone mode:

- in debug mode, se_illegal works like software breakpoint. IVOR6 is not triggered. If you just step the code, it works like nop instruction. If you run the code and the program reaches se_illegal instruction, the device will stop execution and it will enter debug mode.

- if the device is running in standalone without debugger, se_illegal will trigger IVOR6 exception.

0 件の賞賛
返信
2,711件の閲覧回数
20Sidar04
Contributor III

Thanks David for advices. It works. 

0 件の賞賛
返信