PE Driver(multilink_universal_install_12.2 ) can use on CodeWarrior 2.1 IDE ,but it can not use on the CodeWarrior 10.7, it must instatll 12.7. Is PE Driver can used on the both CodeWarrior 2.1 IDE and CodeWarrior 10.7 IDE?
解決済! 解決策の投稿を見る。
Can you try to install P&E patch available here:
https://www.pemicro.com/downloads/download_file.cfm?download_id=463
This should update the support for all compatible PEmicro interfaces into CW MPC55xx/56xx v2.10
Stan
Hi,
I've just installed Drivers 12_7 on my Windows 10 64bit machine and use it with CodeWarrior for MPC55xx/56xx v2.10 and
All configurations work as expected.
Do you observe any issue on your side?
If yes, can you attach the error screenshot?
Hope it helps.
Stan
Hi,
Could you please help me to resolve this error.
PFB is me driver details
The USB indication led is turned on and it is blue color.
Still the software is not detecting the hardware.
Hi,Thank you for your replying. My window is Windows 11 64bit , My drive and PE type is as following figure
When debuging on CodeWarrior 2.10 using multilink_universal_install _12.7. It is not ok,
When debuging on CodeWarrior 2.10 using multilink_universal_install _12.0. It is ok,
Can you try to install P&E patch available here:
https://www.pemicro.com/downloads/download_file.cfm?download_id=463
This should update the support for all compatible PEmicro interfaces into CW MPC55xx/56xx v2.10
Stan
Hi
Thank you, I solved the PEmicro recognition problem using the method above, but now I'm encountering the "load fail" issue.
when I clicked the "connect(Reset)"button ,the new problem was appeared as below. And how can I solve this problem ?(load aborted)
Thank you!
Thank you for your replying