CodeWarrior 2.1 and CodeWarrior 10.6 PE Driver

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

CodeWarrior 2.1 and CodeWarrior 10.6 PE Driver

Jump to solution
1,182 Views
Yorn
Contributor I

PE Driver(multilink_universal_install_12.2 ) can use on CodeWarrior 2.1 IDE ,but  it can not use on the CodeWarrior 10.7, it must instatll 12.7. Is PE Driver can used on the both CodeWarrior 2.1 IDE and CodeWarrior 10.7 IDE?

0 Kudos
Reply
1 Solution
1,057 Views
stanish
NXP Employee
NXP Employee

Can you try to install P&E patch available here:

https://www.pemicro.com/downloads/download_file.cfm?download_id=463

This should update the support for all compatible PEmicro interfaces into CW MPC55xx/56xx v2.10

Stan

View solution in original post

0 Kudos
Reply
9 Replies
1,160 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

@stanish could you comment here?

Best regards,

Peter

0 Kudos
Reply
1,106 Views
stanish
NXP Employee
NXP Employee

Hi, 

I've just installed Drivers 12_7 on my Windows 10 64bit machine and use it with CodeWarrior for MPC55xx/56xx v2.10 and

  • PEmicro Multilink FX (black probe) rev.C
  • PEmicro Multilink PowerPC Nexus (blue probe) rev.

stanish_0-1725886325651.png

All configurations work as expected.

 

Do you observe any issue on your side?

If yes, can you attach the error screenshot?

Hope it helps.

Stan

0 Kudos
Reply
304 Views
ArunMukundan
Contributor I

Hi,

Could you please help me to resolve this error.

ArunMukundan_0-1733385722303.png

 

PFB is me driver details

ArunMukundan_1-1733385776134.png

 

The USB indication led is turned on and it is blue color. 

Still the software is not detecting the hardware.

0 Kudos
Reply
1,090 Views
Yorn
Contributor I

Hi,Thank you for your replying. My window is Windows 11 64bit , My drive and PE type is as following figure

Yorn_0-1725928745017.png 

Yorn_2-1725929907851.png

When debuging on  CodeWarrior 2.10 using multilink_universal_install _12.7. It is not ok,

Yorn_3-1725930239613.png

When debuging on  CodeWarrior 2.10 using multilink_universal_install _12.0. It is  ok,

Yorn_4-1725930353288.png

 

 

 

0 Kudos
Reply
1,058 Views
stanish
NXP Employee
NXP Employee

Can you try to install P&E patch available here:

https://www.pemicro.com/downloads/download_file.cfm?download_id=463

This should update the support for all compatible PEmicro interfaces into CW MPC55xx/56xx v2.10

Stan

0 Kudos
Reply
808 Views
ZhaoDinan
Contributor II

Hi 

ZhaoDinan_0-1728636156338.png

Thank you, I solved the PEmicro recognition problem using the method above, but now I'm encountering the "load fail" issue.

when I clicked the "connect(Reset)"button ,the new problem was appeared as below. And how can I solve this problem ?(load aborted)

ZhaoDinan_1-1728636195461.png

 

0 Kudos
Reply
800 Views
Yorn
Contributor I
IT is not found elf.file ,reload the elf file to the path
0 Kudos
Reply
766 Views
ZhaoDinan
Contributor II

Thank you!

0 Kudos
Reply
1,041 Views
Yorn
Contributor I

Thank you for your replying

0 Kudos
Reply