Clock Monitor Unit in MPc5604s

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Clock Monitor Unit in MPc5604s

4,410 Views
mhogun
Contributor I

Hi All,

I am trying to change the CMU_CSR register by the following values,but the register is not changed .

/* RC clock division factor */
CGM.CMU_CSR.B.RCDIV = 2;

/* Enable clock monitor bit */
CGM.CMU_CSR.B.CME_A = BIT_SET;

/* Start frequency measure */
CGM.CMU_CSR.B.SFM = BIT_SET;

/*RC Oscillator(s) selection bit */
CGM.CMU_CSR.B.CLKSEL1 = 0;


CGM.CMU_MDR.B.MD = 256;

0 Kudos
Reply
6 Replies

3,747 Views
janos_murai
Contributor III

Hello,

could you solve this? 

I have a similar issue, but with an MPC5645S.

Thank you!

János Murai

0 Kudos
Reply

3,747 Views
mhogun
Contributor I

Hi Peter,

I have checked the write protection also. It is disabled after reset hence it is not the issue. I am also not able to change the values of High Frequency Reference Register FMPLL0(CMU_HFREFR_A) and Low Frequency Reference Register FMPLL0(CMU_LFREFR_A). 

Thanks in advance

Mohanraj

0 Kudos
Reply

3,747 Views
petervlna
NXP TechSupport
NXP TechSupport

Hi,

I am able to modify it with any issues.

Are you sure you are running system with enabled XOSC and PLL which you want to monitor.

Because without it you cannot write to CMU as there is no valid reference frequency for CMU comparison.

Run one of our examples with PLL as system clock and then change CMU values in debugger to see if it change.

For example I have used:https://community.nxp.com/docs/DOC-331807 

Peter

0 Kudos
Reply

3,747 Views
mhogun
Contributor I

Hi All,

I am trying to change the CMU_CSR register by the following values,but the register is not changed .

 

/* RC clock division factor */
CGM.CMU_CSR.B.RCDIV = 2;

/* Enable clock monitor bit */
CGM.CMU_CSR.B.CME_A = BIT_SET;

/* Start frequency measure */
CGM.CMU_CSR.B.SFM = BIT_SET;

/*RC Oscillator(s) selection bit */
CGM.CMU_CSR.B.CLKSEL1 = 0;


CGM.CMU_MDR.B.MD = 256;

Kindly help me to change the register.

I need to monitor the crystal clock and PLL clock.

Also support me to use Clock monitor unit in the controller.

0 Kudos
Reply

3,747 Views
petervlna
NXP TechSupport
NXP TechSupport

Hello,

This is strange, as the register is writable:

pastedImage_1.png

What comes to my mind is:

1. The writes are protected via register protection mechanism. Are you setting register protection?

2. The header file addresses of CMU are incorrect

Can you see in debugger that your code in assembly is writing to location of CMU_CSR correctly and it is still not updated??

Peter

0 Kudos
Reply

3,747 Views
mhogun
Contributor I

Hi Peter,

I have checked header files it is seems to be correct.

May be because of write protection i am not able to write the rsgister.

Please help me to unlock the write protection of CMU_CSR register

0 Kudos
Reply