CAN-FD Example

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

CAN-FD Example

1,093 次查看
ognyanyanchev
Contributor I

Hello,

I have question about CAN-FD example MPC5748G-FlexCAN_FD-TX_RX-test-GHS614.

When I try to execute it the CAN_0 and CAN_1 initialization performed OK, but when I try to send message

over the bus the send sequence stops always  on the flags check line.

The question is:

Is somebody have the same problem and can help me to solve the problem..

For information I use the following:

MCU:   SPC5748GGMMJ6 1N81M on the Demo Board.

Header file: from example, because my original header file MPC5748G_4.0.01_1N81M.h, but it not contain

                    information about CAN-FD settings EDL, BRS, ESI.

0 项奖励
回复
0 回复数