CAN-FD Example

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

CAN-FD Example

1,115件の閲覧回数
ognyanyanchev
Contributor I

Hello,

I have question about CAN-FD example MPC5748G-FlexCAN_FD-TX_RX-test-GHS614.

When I try to execute it the CAN_0 and CAN_1 initialization performed OK, but when I try to send message

over the bus the send sequence stops always  on the flags check line.

The question is:

Is somebody have the same problem and can help me to solve the problem..

For information I use the following:

MCU:   SPC5748GGMMJ6 1N81M on the Demo Board.

Header file: from example, because my original header file MPC5748G_4.0.01_1N81M.h, but it not contain

                    information about CAN-FD settings EDL, BRS, ESI.

0 件の賞賛
返信
0 返答(返信)