C90FL Flash erase Question

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

C90FL Flash erase Question

Jump to solution
5,204 Views
youngguekim
Contributor II

Hi. I am using MPC5644A and want to erase Flash memory by using C90FL Driver.

 

FlashErase have Parameters(in) : lowEnabledBlocks, midEnabledBlocks, highEnabledBlock.

 

I don't know What I should put a data in lowEnabledBlocks, midEnabledBlocks, highEnabledBlock.

 

 

lowEnableBlocks

M1

M0

L9

L8

L7

L6

L5

L4

L3

L2

L1

L0

data

0

0

0

0

0

0

0

0

0

0

0

0

midEnabledBlocks

 

 

 

 

 

 

 

 

 

 

M0

L0

data

 

 

 

 

 

 

 

 

 

 

0

0

highEnabledBlock

 

 

 

 

 

H6

H5

H4

H3

H2

H1

H0

data

 

 

 

 

 

0

0

0

0

0

0

0

 

is it right????

 

if i want to erase 0x4000 Block, 0x1_0000 block, 0x0004_0000 block, 0x00C_0000 block, 0x0020_0000 block

What should I deal with lowEnabledBlocks, midEnabledBlocks, highEnabledBlock Parameters

 

 

MPC5644A flash memory 

 

166539_166539.pngpastedImage_1.png

 

 

 

FlashErase Function

 

166540_166540.pngpastedImage_2.png

Labels (1)
0 Kudos
Reply
1 Solution
4,877 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

No, it is not. With using of SSD driver, user uses logical address mapping. midEnabledBlock has only 2 bits.

pastedImage_1.png

View solution in original post

6 Replies
4,877 Views
youngguekim
Contributor II

I tried to erase Flash memory '0x3_0000~ 40_0000' to use Function 'pFlashErase'   (0x0000~0x3_0000 is Bootloader)

I set 

lowEnabledBlocks = 0xE00 = 0b1110_0000_0000

midEnabledBlocks = 0x3 = 0b11

highEnabledBlock = 0x3F = 0b11_1111

but the area '0x4_0000~0x6_0000' and 0x3F_0000..' is not erased..(check it by trace32)

I tried again 

lowEnabledBlocks = 0xFFFF_FFFF 

midEnabledBlocks = 0xFFFF_FFFF 

highEnabledBlock = 0xFFFF_FFFF 

and the area '0x4_0000~0x6_0000' and 0x3F_0000..' is erased exactly.

What is the problem??

Thank you for your help

0 Kudos
Reply
4,877 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

I have just it and it works normally to me.

lowEnabledBlocks = 0x0E00 followed by erase sequence erases 0x0003_0000-0x0007_FFFF

I don't see any issue.

0 Kudos
Reply
4,877 Views
youngguekim
Contributor II

Thank you very much

it works well

0 Kudos
Reply
4,877 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

Yes, it is right if you mean physical to logical address mapping.
Only I would note that the logical block is being selected by logic 1 in the particular bit-mapped position.

0 Kudos
Reply
4,877 Views
youngguekim
Contributor II

midEnabledBlock is L0 and M0 of Flash B??

As you say, midEnabledBlock is just 2 bit ??

but in Datasheet MPC5644A

High-Address Space Block Select Register is 10bit

Mid-Address Space Block Select Register is 2bit

Low-Address Space Block Select Register is 6bit

is this not relevant????

pastedImage_1.png

0 Kudos
Reply
4,878 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

No, it is not. With using of SSD driver, user uses logical address mapping. midEnabledBlock has only 2 bits.

pastedImage_1.png