Byte Craft eTPU Compiler

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Byte Craft eTPU Compiler

2,952件の閲覧回数
NAIDU
Contributor III

Hi All,

  We had purchased byte craft compiler for MPC5554. Now can we use same Byte Craft compiler for MPC5777C. is there any difference?

Thanks&Regards,

Naidu.

3 返答(返信)

2,767件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

It is rather question for Bytecraft, but how it was already told here, eTPU2 is backward compatible with eTPU.

 

I could recommend another third-party tools:

ETPU Tools | Website | Ashware

0 件の賞賛
返信

1,871件の閲覧回数
EmilyZhou8
Contributor III

Hi 

I am wondering if I want to generate "auto.h" file for function application and edit "set.h" file, should buy both eTPU2+ Development Tool and ETEC C Compiler? And I also want to know the differenec between with and without network licence. 

EmilyZhou8_0-1725851900559.png

 

Thank you very much!

Best Regards,

Rongbo

0 件の賞賛
返信

2,767件の閲覧回数
mc6808
Contributor II

The eTPU2+ is bacwards compatible so you can use existing tools, but unless the bytecraft compiler has improved radically it was not really compatible with any eTPU: the version I used was full of bugs.