Byte Craft eTPU Compiler

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Byte Craft eTPU Compiler

2,946 Views
NAIDU
Contributor III

Hi All,

  We had purchased byte craft compiler for MPC5554. Now can we use same Byte Craft compiler for MPC5777C. is there any difference?

Thanks&Regards,

Naidu.

3 Replies

2,761 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

It is rather question for Bytecraft, but how it was already told here, eTPU2 is backward compatible with eTPU.

 

I could recommend another third-party tools:

ETPU Tools | Website | Ashware

0 Kudos
Reply

1,865 Views
EmilyZhou8
Contributor III

Hi 

I am wondering if I want to generate "auto.h" file for function application and edit "set.h" file, should buy both eTPU2+ Development Tool and ETEC C Compiler? And I also want to know the differenec between with and without network licence. 

EmilyZhou8_0-1725851900559.png

 

Thank you very much!

Best Regards,

Rongbo

0 Kudos
Reply

2,761 Views
mc6808
Contributor II

The eTPU2+ is bacwards compatible so you can use existing tools, but unless the bytecraft compiler has improved radically it was not really compatible with any eTPU: the version I used was full of bugs.