Bootloader And Application PIT Clock Problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Bootloader And Application PIT Clock Problem

2,327 Views
erreer
Contributor II

       My bootloader works correct, The application to be bootloaded works correct on it's own when is it programmed directly onto the micro. When I bootload the application with the bootloader and jump direct to the application from the bootloader I have the following problem:

(1)   PIT time is wrong  

Bootloader clock configuration (not use PIT ) :

void Sys_Init(void)
{
//Clk Out
MC_CGM.AC6_SC.R = 0x02000000; //Enable PLL0 - clkout0 //MC_CGM_AC6_SC
MC_CGM.AC6_DC0.B.DE = 1; //Enable divider for SYSCLK0
MC_CGM.AC6_DC0.B.DIV = 3; //Set divider for SYSCLK0 (div by 4)

//Configure RunPeripheralConfiguration regist ers in ME_RUN_PC0
MC_ME.RUN_PC[0].B.DRUN = 1; //Enable DRUN mode for all peripherals using ME_RUN_PC[0]

MC_ME.DRUN_MC.B.XOSCON = 1; //Enable external oscilator

//AUX Clock Selector 3 setup
MC_CGM.AC3_SC.B.SELCTL =0x01; //connect (8..40MHz) XTALL to the PLL0 input
MC_ME.DRUN_MC.B.PLL0ON = 1; //Enable PLL0 for DRUN mode

//AUX Clock Selector 0 setup
MC_CGM.AC0_SC.B.SELCTL=0x2; //source PLL0 PHI 200MHz
MC_CGM.AC0_DC0.R = 0x80010000; //MOTC_CLK enable with divider 1
MC_CGM.AC0_DC2.R = 0x80010000; //ADC_CLK enable with divider 1

// Set PLL0 to 200MHz
PLLDIG.PLL0CR.B.CLKCFG = 1; //Bypass mode PLL0 on
// RFDPHI1 = 10, RFDPHI = 2, PREDIV = 2, MFD = 14
PLLDIG.PLL0DV.R = 0x50000000 |0x00020000 |0x00002000 |0x0014 ; //predefined PLL0 divider register

//Mode transition to apply the PLL0 setup and set Normal mode with PLL running
MC_ME.MCTL.R = 0x30005AF0; //DRUN Mode & Key
MC_ME.MCTL.R = 0x3000A50F; //DRUN Mode & Key

while(!MC_ME.GS.B.S_PLL0); //ME_GS Wait for PLL stabilization.
while(MC_ME.GS.B.S_MTRANS); //Waiting for end of transaction
while(MC_ME.GS.B.S_CURRENT_MODE != DRUN_MODE); // ME_GS Check DRUN mode has successfully been entered
}//Sys_Init

Application clock configuration :

 MC_ME.RUN_PC[0].R=0x000000FE;//

void Sys_Init_1(void)
{
MC_ME.RUN0_MC.R&=0xFFFFFF1F; //


/* Configure PLL0 to 160 MHz. */
PLLDIG.PLL0DV.B.RFDPHI1 = 4;
PLLDIG.PLL0DV.B.RFDPHI = 4;
PLLDIG.PLL0DV.B.PREDIV = 1;
PLLDIG.PLL0DV.B.MFD = 16;

//Fpll1_phi=80Mhz
PLLDIG.PLL1DV.B.RFDPHI = 10;
PLLDIG.PLL1DV.B.MFD = 10;


MC_CGM.AC3_SC.B.SELCTL=1; 
MC_CGM.AC4_SC.B.SELCTL=3; 


MC_CGM.SC_DC0.B.DIV = 3; /* Freq = sysclk / (3+1) = sysclk / /20MHZ 
MC_CGM.SC_DC0.B.DE = 1; /* Enable divided clock */


MC_CGM.AC0_SC.B.SELCTL=0;
//MC_CGM.AC0_SC.B.SELCTL=1;
MC_CGM.AC0_DC0.R = 0x80000000|(AUX0_clk_DIV0 <<16); 
MC_CGM.AC0_DC2.R=0x80010000;

MC_ME.RUN0_MC.R|=0x00000020; //
MC_ME.RUN0_MC.R|=0x00000040; /
MC_ME.RUN0_MC.R|=0x00000080; //
MC_ME.RUN0_MC.R|=0x00000004; //80M


MC_ME.MCTL.R = 0x40005AF0;
MC_ME.MCTL.R = 0x4000A50F;
while(MC_ME.GS.B.S_MTRANS == 1); /* Wait for mode transition complete */
while(MC_ME.GS.B.S_CURRENT_MODE!=4); //

}//Sys_Init

 MC_ME.PCTL30.B.RUN_CFG = 0; // PIT

PIT_0.MCR.B.MDIS = 0; // 
PIT_0.MCR.B.FRZ = 1; // 
PIT0_init(1999999); // 100MS
PIT_0.MCR.B.FRZ = 0; //

I find that the clock of PIT is IRCOSC, I do this in bootloader when jump to application  but it is not work.

Bootloader :

MC_ME.RUN_PC[1].B.DRUN =0; 

 MC_ME.PCTL30.B.RUN_CFG = 1; 

PIT_0.MCR.B.MDIS = 1; 

Labels (1)
Tags (1)
0 Kudos
Reply
1 Reply

2,221 Views
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

I'm used to recommend these two things:

- either jump to the application right after reset

- or put everything back to default reset state in bootloader before jumping to the application.

This is 100% solution for all similar issues.

Regards,

Lukas