BAM problem: RAppID boot loader error (MPC 5644a)

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

BAM problem: RAppID boot loader error (MPC 5644a)

3,662件の閲覧回数
aperico
Contributor I

Hi,

 

I am having problems to flash over CAN using BAM.

Below is the error message I get from the RAppID gui:

63277_63277.PNGCapture.PNG

Error message

"Loss Communication with BAM at Password. Check that Password is correct."

"Password Verification failure"

"Initialization
Error with BAM. Check Password or Verify Boot Configuration Setting
ABS2=1, ABS0=0, FAB=1, Please cycle power and try again."

 

Our code works normally when flashed over a "universal programmer" (debugging), but we need to be able to flash over CAN (CANCase XL).

* We have FlexCAN0 and FlexCAN1 activated.

 

I have tried the suggestions from the posts below, but so far, no success:

RAppID boot loader error

Rappid error - cannot boot from CAN with autobaud

Boot Assist Module (BAM) with FlexCAN MPC5604P

 

 

 

From what I understood, I just have to add the following in my code (to enable BAM), is this really all I need to do ?

I cannot understand more than that from the documentation.

 

-----------------------------------

#define RSTCFG_PCR 210

#define BOOTCFG0_PCR 211

#define BOOTCFG1_PCR 212

...

main(void) {

     // BAM -------------------------------

     PCR[BOOTCFG0_PCR].B.PA = 1;

     PCR[BOOTCFG1_PCR].B.PA = 1;

     PCR[BOOTCFG0_PCR].B.IBE = 0; // ABS0

     PCR[BOOTCFG1_PCR].B.IBE = 1; // ABS2

     RSR.B.BOOTCFG = 0x01;

     PCR[RSTCFG_PCR].B.PA = 1;

     PCR[RSTCFG_PCR].B.IBE = 0;

... (our normal application code)...

}

-----------------------------------

   
 
 
 
 
 
 
 
 
 
 
 





ラベル(1)
タグ(5)
0 件の賞賛
返信
3 返答(返信)

3,049件の閲覧回数
alessandrosirto
Contributor II

Hi , 

I have saw  this discussion and I' m intersted about it. A part of the hardware configuration of BOOTCFG pins , Can you only confirm that the RAppID Boot Loader Utility works with the Vector Can Case XL for the MPC5644A? I ask you because before buy that I want to be sure as mauch as possible that there is no bug o problem to use that type of setting for booloading .

Thanks in advance ,

Alessandro.  

0 件の賞賛
返信

3,049件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi Alessandro,

yes, Vector CAN Case XL is supported, I'm not aware of issues.

But notice that this tool from Vector is not available anymore. It was replaced by VN1600 devices. I got information from SW team that it's backward compatible and it works too.

Regards,

Lukas

0 件の賞賛
返信

3,049件の閲覧回数
lukaszadrapa
NXP TechSupport
NXP TechSupport

Hi,

you can't enable the BAM by software. ABS2, ABS0 and FAB pins or BOOTCFG pins (depends on device) must be configured on hardware level - it is necessary to tie the pins to required voltage level. The state of these pins is read during reset, so they cannot be set by software.

Regards,

Lukas

0 件の賞賛
返信