Atuosar generates a configuration file, how to manually import S32DS GON

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Atuosar generates a configuration file, how to manually import S32DS GON

3,061件の閲覧回数
lubo_NEW
Contributor III

Your technology says that AUTOSAR cannot be compiled with S32DS, but only with GCC compiler.
But is there another way to manually configure the generated files to generate executable code in S32DS
Or how to directly generate AUTOSAR code in the form of C library files in S32DS directly
thank you

0 件の賞賛
返信
7 返答(返信)

2,237件の閲覧回数
pt77
Contributor I

Hello,Do you use S32DS compile Davinci Configurator Generated Code?I just do it now,but i done not how to Do,Can you give some support to me?

0 件の賞賛
返信

3,047件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hello,

For MPC5xxx there is only GHS and Windriver supported.

But if you are talking about S32Kxx then also gcc (S32DS) is supported.

Which micro are you referring to specifically?

best regards,

Peter

 

0 件の賞賛
返信

3,045件の閲覧回数
lubo_NEW
Contributor III

Can AUTOSAR_OS build an SDK package like freertos and compile directly on S32DS without EB Tresos generation code

0 件の賞賛
返信

3,040件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hello,

 

AUTOSAR OS configuration must be generated from Tresos.

There is AUOTSAR OS makefile project supplied, I recommend you to have a look at it.

 

best regards,
Peter

0 件の賞賛
返信

3,035件の閲覧回数
lubo_NEW
Contributor III

That folder is the generated code that EB Tresos got, I can't find it   Thank you for your replynn22.png

0 件の賞賛
返信

3,029件の閲覧回数
lubo_NEW
Contributor III

Thank you for your reply. I haven't found many of the OS examples you mentioned, or reference examples or generated configuration files.
I want to add the generated configuration file into the DS32DS project manually.
I looked at the generated files and configuration files and some of them did not seem to have a description like the EVENT

 

no1.pngNO2.png

0 件の賞賛
返信

3,032件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hello,

The Tresos only generate configuration files. It is customer responsibility to put them into a project.

For example into OS demo.

Best regards,

Peter

0 件の賞賛
返信