Application notes on external bus usage for the MPC5777C

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Application notes on external bus usage for the MPC5777C

ソリューションへジャンプ
2,417件の閲覧回数
prathapvc
Contributor III

Most the ANs and reference designs are targeting the usage of the embedded peripherals of the powertrain family of MCUs, not the EBI. Can one point me out to some literature like the interfacing to External NOR Flash and SRAM using EBI but targeted to the MPC5777C

1 解決策
2,154件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

I could point out my document shared on community answering typical customer question related to external bus:
External Bus Interface FAQs 

EBI appnote also exists, however it does not cover the whole functionality as it is intended for MPC5510:
https://www.nxp.com/docs/en/application-note/AN3773.pdf 

Otherwise I could answer specific details here over community thread or over customers cases:
https://community.nxp.com/docs/DOC-329745 

元の投稿で解決策を見る

2 返答(返信)
2,155件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

I could point out my document shared on community answering typical customer question related to external bus:
External Bus Interface FAQs 

EBI appnote also exists, however it does not cover the whole functionality as it is intended for MPC5510:
https://www.nxp.com/docs/en/application-note/AN3773.pdf 

Otherwise I could answer specific details here over community thread or over customers cases:
https://community.nxp.com/docs/DOC-329745 

2,154件の閲覧回数
prathapvc
Contributor III

Ok thank you