What is the meaning of “PARTITION” in MPC5645S

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

What is the meaning of “PARTITION” in MPC5645S

Jump to solution
1,534 Views
hyacinth
Contributor II

Dear All,

In the description of Flash for MPC5645S,L0 to L3 are located in Patition 1,L4 to L7 are located in Patition 2...

When erase the Blocks,is there anything special within a patition?And What is the physical Meaning of  Patition here?

pastedImage_1.png

BR

Chen

Labels (1)
1 Solution
1,056 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

Hi, code may be executed from one partition while another one is being programmed. That's the reason for flash partitions.

View solution in original post

4 Replies
1,057 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

Hi, code may be executed from one partition while another one is being programmed. That's the reason for flash partitions.

1,056 Views
hyacinth
Contributor II

So,when the code is executed from L1 and L2, it is not allowed to program L3?

0 Kudos
Reply
1,056 Views
davidtosenovjan
NXP TechSupport
NXP TechSupport

You are right.

1,056 Views
hyacinth
Contributor II

Thanks for your reply, it's sloved the problem perfectly!

0 Kudos
Reply