About reset escalation

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

About reset escalation

1,820件の閲覧回数
Questioner
Contributor II

How does the mpc5748g board goes into reset escalation mode.

I didnot press any reset button while the code is compiling.

0 件の賞賛
返信
1 返信

1,807件の閲覧回数
petervlna
NXP TechSupport
NXP TechSupport

Hello,

I am not sure what you are doing. To be sure you see reset escalation you can measure the reset pin by scope after power on reset. If it toggles then you have reset escalation cause by SWT in majority of the times.

This is the case when you have fresh sample, we enable SWT by default in NXP fab for 20ms.

If you have for example Lauterbach debugger you can use the "halt core on power on reset"script from drop menu.

In case of PE you can have a look at here:

https://community.nxp.com/t5/MPC5xxx/MPC5748G-Reset-escalation-PEMicro-Multilink-FX/m-p/951221

 

Here is how the reset escalation looks like on scope and also solution:

https://community.nxp.com/t5/MPC5xxx/MPC5746C-enter-reset-escalation/m-p/750582

 

best regards,

Peter

0 件の賞賛
返信