ASIL D for MPC5777C

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
2,793件の閲覧回数
berat24
Contributor III

Hello everyone,

MPC5777C supports realibity up to ASIL D powertrain. How can we prove that We use ASIL-D supported features of the MCU?

MPC5xxx Microcontrollers | NXP Semiconductors

0 件の賞賛
返信
1 解決策
2,777件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

Functional safety and the ISO26262 standard define the general guidelines needed to fulfill the requirements for the different ASIL levels. In NXP we have a program called safe assure. For more information about this program and the devices see following link:

https://www.nxp.com/products/product-information/functional-safety-for-iso-26262-and-iec-61508:FNCTN...

“The SafeAssure program highlights selected solutions - including hardware and software - that are targeted for use in functional safety applications, enabling system designers to design with confidence and achieve their system-level design goals and standards compliance more efficiently.”

ASIL certification is being above whole ECU/system level, so customer could develop ASIL-D compliant appliance with MPC5777C (he could also develop ASIL-D compliant appliance with other devices than safety certified, but such approach could be in-efficient, slow, expensive, complicated, and so on…)

It means not only MCU is designed and manufactured according ISO26262 requirements (safety HW) but also we are providing safety software and safety support (documents) as stated on the link above.

Here you may find procedure how to obtain safety documents:

https://community.nxp.com/t5/SafeAssure-Community/bd-p/safeassure

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
2,778件の閲覧回数
davidtosenovjan
NXP TechSupport
NXP TechSupport

Functional safety and the ISO26262 standard define the general guidelines needed to fulfill the requirements for the different ASIL levels. In NXP we have a program called safe assure. For more information about this program and the devices see following link:

https://www.nxp.com/products/product-information/functional-safety-for-iso-26262-and-iec-61508:FNCTN...

“The SafeAssure program highlights selected solutions - including hardware and software - that are targeted for use in functional safety applications, enabling system designers to design with confidence and achieve their system-level design goals and standards compliance more efficiently.”

ASIL certification is being above whole ECU/system level, so customer could develop ASIL-D compliant appliance with MPC5777C (he could also develop ASIL-D compliant appliance with other devices than safety certified, but such approach could be in-efficient, slow, expensive, complicated, and so on…)

It means not only MCU is designed and manufactured according ISO26262 requirements (safety HW) but also we are providing safety software and safety support (documents) as stated on the link above.

Here you may find procedure how to obtain safety documents:

https://community.nxp.com/t5/SafeAssure-Community/bd-p/safeassure

0 件の賞賛
返信