33907 wake up problem

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

33907 wake up problem

跳至解决方案
2,199 次查看
liujinhang
Contributor III

hi,

I have a question about 33907 wake up machanism. see below:

160136_160136.bmpIO_0.bmp

precondition is IO_0 has been configured to be "rising edge wake up 33907".

if MCU program will make 33907 go to sleep by sending an "go to sleep" SPI command. but at this time IO_0 has been high state. 

if the IO_0 high state maintains, can 33907 be wake up?    if 33907 can not be wake up, how can we do to confirm every time of going into sleep mode can be wake up by an rising edge of IO_0.

from up figure, we can see MCU program cannot make sure send "go to sleep" command of SPI before IO_0 rising edge.

标签 (1)
1 解答
1,950 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Liu,

We know of this weakness which is by the way corrected on FS6500 family. The workaround is proposed in the AN5766, chapter 6.2 - extracted below:

cp1.png

cp2.png

Best regards,

Tomas

PS: If this answer helps to solve your question, please mark it as "Correct". Thank you.

在原帖中查看解决方案

1 回复
1,951 次查看
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Liu,

We know of this weakness which is by the way corrected on FS6500 family. The workaround is proposed in the AN5766, chapter 6.2 - extracted below:

cp1.png

cp2.png

Best regards,

Tomas

PS: If this answer helps to solve your question, please mark it as "Correct". Thank you.