33907 wake up problem

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

33907 wake up problem

Jump to solution
2,200 Views
liujinhang
Contributor III

hi,

I have a question about 33907 wake up machanism. see below:

160136_160136.bmpIO_0.bmp

precondition is IO_0 has been configured to be "rising edge wake up 33907".

if MCU program will make 33907 go to sleep by sending an "go to sleep" SPI command. but at this time IO_0 has been high state. 

if the IO_0 high state maintains, can 33907 be wake up?    if 33907 can not be wake up, how can we do to confirm every time of going into sleep mode can be wake up by an rising edge of IO_0.

from up figure, we can see MCU program cannot make sure send "go to sleep" command of SPI before IO_0 rising edge.

Labels (1)
1 Solution
1,951 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Liu,

We know of this weakness which is by the way corrected on FS6500 family. The workaround is proposed in the AN5766, chapter 6.2 - extracted below:

cp1.png

cp2.png

Best regards,

Tomas

PS: If this answer helps to solve your question, please mark it as "Correct". Thank you.

View solution in original post

1 Reply
1,952 Views
TomasVaverka
NXP TechSupport
NXP TechSupport

Hi Liu,

We know of this weakness which is by the way corrected on FS6500 family. The workaround is proposed in the AN5766, chapter 6.2 - extracted below:

cp1.png

cp2.png

Best regards,

Tomas

PS: If this answer helps to solve your question, please mark it as "Correct". Thank you.