******************************************************************************** * Detailed Description: * This example shows, how to use interrupt hardware vector mode. In the example * PIT0 interrupt and external interrupt source 1 are implemented. PIT interrupt * toggle LED every second, external interrupt causes IVOR1 exception. * * This example also shows, how to use exceptions, while HW vector mode is used. * After SW1 button is pressed, uninitialized RAM is read and IVOR1 exception is * reached. In IVOR1, only endless loop is implemented and micro has to be reset * externally if you want to get out from this loop. * * * For correct HW vector mode setup, following files was added to the project: * * - exceptions.s * - handlers_vle.s * - HW_vector.c * * * Following files was modified (all changes are marked by comment): * * - mem.ld * - sections.ld * - Vector.c * - MPC57xx__Interrupt_Init.c * * * Following files was removed from project (files are still place in project, but * not compiled and linked) * * - intc_sw_handlers.S * - intc_SW_mode_isr_vectors_MPC5744P.c * * * * Test HW: X-MPC5744P-144DC, MPC57xx motherboard * MCU: PPC5744PFMLQ8 0N15P * Fsys: 200 MHz * Debugger: Lauterbach Trace32 * PeMicro USB-ML-PPCNEXUS * Target: internal_FLASH (debug mode, release mode) * EVB connection: User LED 1 connected to A0 (P8.0), * User switch SW1 connected to A1 (P8.1) * * * ------------------------------------------------------------------------------ * ********************************************************************************
記事全体を表示