Example MPC5604B SWT Windowed mode CW110

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Example MPC5604B SWT Windowed mode CW110

Example MPC5604B SWT Windowed mode CW110

********************************************************************************
* Detailed Description:
* Application performs basic initialization, setup PLL to maximum allowed freq.,
* initializes interrupts and initializes software watchdog with window mode
* allowed. Window mode is set for 2.5 ms. PIT timer is set to service SWT each
* 8 ms, which is inside the window.
*
*
* ------------------------------------------------------------------------------
* Test HW:         XPC560B 100LQFP, XPC56XX EVB MOTHEBOARD Rev.C
* MCU:             PPC5604BE MLL 1M27V
* Fsys:            64 MHz
* Debugger:        Lauterbach Trace32
*                  PeMicro USB-ML-PPCNEXUS
* Target:          RAM, internal_FLASH
* EVB connection:  
*
********************************************************************************

添付
評価なし
バージョン履歴
最終更新日:
‎01-21-2019 01:17 AM
更新者: