Example MPC5604B SWT Windowed mode CW110

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Example MPC5604B SWT Windowed mode CW110

Example MPC5604B SWT Windowed mode CW110

********************************************************************************
* Detailed Description:
* Application performs basic initialization, setup PLL to maximum allowed freq.,
* initializes interrupts and initializes software watchdog with window mode
* allowed. Window mode is set for 2.5 ms. PIT timer is set to service SWT each
* 8 ms, which is inside the window.
*
*
* ------------------------------------------------------------------------------
* Test HW:         XPC560B 100LQFP, XPC56XX EVB MOTHEBOARD Rev.C
* MCU:             PPC5604BE MLL 1M27V
* Fsys:            64 MHz
* Debugger:        Lauterbach Trace32
*                  PeMicro USB-ML-PPCNEXUS
* Target:          RAM, internal_FLASH
* EVB connection:  
*
********************************************************************************

附件
无评分
版本历史
最后更新:
‎01-21-2019 01:17 AM
更新人: