imxrt1170 EVK, LCD display interface SDK example

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

imxrt1170 EVK, LCD display interface SDK example

1,461 Views
srihari
Contributor I

I have MIMXRT1170 EVK  board.

Using MCUxpress IDE, imported the SDK, in SDK have ran  the hello world and led blinky example projects which is available, working fine build, flash and debug.
same thing in SDK selected the existing example for display 

 

2026-04-08_10h57_33.png2026-04-08_10h58_15.png

this memory configs are not modified used the existing only, 
here able to build and able to flash,
here my debug configurations are 2026-04-08_11h01_51.png
Here issue is when i do debug i am facing bus fault errors and hard fault error, as you can see in image 
 2026-04-08_11h03_53.png
Can someone suggest any memory configs need to do, any debug configurations need to modify 
@lcdguru @Displays 

Labels (2)
Tags (1)
0 Kudos
Reply
2 Replies

1,372 Views
Gavin_Jia
NXP TechSupport
NXP TechSupport

Hi @srihari ,

Thanks for your interest in NXP MIMXRT series!

Could you provide me with some more information?
The SDK version number and the IDE version number. Also, are you using the on-board debugger? Are you using CMSIS-DAP firmware? What is the EVK board power supply configuration?

This information will help me try to reproduce and diagnose the issue on my end. Thanks in advance!

Best regards,
Gavin

0 Kudos
Reply

1,365 Views
srihari
Contributor I

Hi @Gavin_Jia,
Issue is resolved,
Actually i am using MIMXRT1170-EVKB board but, the SDK I have downloaded for SDK_26.03.00_MIMXRT1170-EVK , it suppose to be SDK_26.03.00_MIMXRT1170-EVKB After downloading the correct SDK, I have executed the display examples, it is working fine 

0 Kudos
Reply