[imx8qm] usb otg2 configuration

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

[imx8qm] usb otg2 configuration

1,084件の閲覧回数
hihanna
Contributor II

Hello

I'm developing it for imx8qm and I'd like to set usbotg2 to peripheral (device) mode.

I think I need to write "Target Controller Driver", is there a document or file that I can refer to? 

And if anyone knows how to set up a dts file, please let me know.

(The circuit is designed as follows.)

hihanna_1-1715923082503.png

 

 

ラベル(1)
  • USB

0 件の賞賛
返信
1 返信

1,064件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

The i.MX8QM application processor has a specified USB3/USB2 OTG module to perform USB 3.0 dual-
role and USB 2.0 On-The-Go (OTG) compatible with the USB 3.0 specification. The processor has an
additional separate, independent USB 2.0 OTG controller which can be used simultaneously with this
USB 3.0.

In our reference design we use the USB2 support dual role you can refer to.

0 件の賞賛
返信