[imx8qm] usb otg2 configuration

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

[imx8qm] usb otg2 configuration

978 Views
hihanna
Contributor II

Hello

I'm developing it for imx8qm and I'd like to set usbotg2 to peripheral (device) mode.

I think I need to write "Target Controller Driver", is there a document or file that I can refer to? 

And if anyone knows how to set up a dts file, please let me know.

(The circuit is designed as follows.)

hihanna_1-1715923082503.png

 

 

Labels (1)
0 Kudos
Reply
1 Reply

958 Views
Rita_Wang
NXP TechSupport
NXP TechSupport

The i.MX8QM application processor has a specified USB3/USB2 OTG module to perform USB 3.0 dual-
role and USB 2.0 On-The-Go (OTG) compatible with the USB 3.0 specification. The processor has an
additional separate, independent USB 2.0 OTG controller which can be used simultaneously with this
USB 3.0.

In our reference design we use the USB2 support dual role you can refer to.

0 Kudos
Reply