evkbmimxrt1170_ota_mcuboot_client_enet fails to load image

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

evkbmimxrt1170_ota_mcuboot_client_enet fails to load image

跳至解决方案
3,500 次查看
drb55
Contributor III

 

Hi,

Followed the Readme carefully, but the last step failed. The signed binary file downloaded from the PC but did not move to the primary slot after reboot as expected. For some reason the Bootloader thinks the image is faulty and erased it.

Used both padded and unpadded images.

python imgtool.py sign --key C:\nxp\IMXRT\SDK_2_15_100_MIMXRT1170-EVKB\boards\evkbmimxrt1170\ota_examples\mcuboot_opensource\cm7\keys\sign-rsa2048-priv.pem --align 4 --header-size 0x400 --pad-header --slot-size 0x200000 --max-sectors 800 --version "1.18.0" C:\Users\geo15\Documents\MCUXpressoIDE_11.9.0_2144\workspace\evkbmimxrt1170_ota_mcuboot_client_enet\Debug\evkbmimxrt1170_ota_mcuboot_client_enet.bin ota.bin --pad --confirm

Possible solutions?

Terminal output.

OTA HTTPS client demo (Ethernet)
Initializing PHY...
Obtaining IP address from DHCP...

************************************************
OTA HTTPS Client Example
************************************************
IPv4 Address : 10.1.15.164

IPv4 Subnet mask : 255.255.255.0

IPv4 Gateway : 10.1.15.1
************************************************

Copyright 2022 NXP

$ ota 0 /ota.bin 10.1.15.119 4433

Started OTA with:
image = 0
file = /ota.bin
host = 10.1.15.119
port = 4433

. Seeding the random number generator...
. Loading the CA root certificate... ok (0 skipped)
. Loading the client cert. and key... ok
. Connecting to 10.1.15.119:4433
. Setting up the SSL/TLS structure... ok
. SSL state connect : 0
. Performing the SSL/TLS handshake...
[ Protocol is TLSv1.2 ]
[ Ciphersuite is TLS-ECDHE-RSA-WITH-AES-256-GCM-SHA384 ]
[ Record expansion is 29 ]
. Verifying peer X.509 certificate... SKIPPED

Getting size of requested file '/ota.bin'
Determined file size is 255016 bytes
Starting download of 255016 bytes with block size of 4096 bytes
...............................................................
Download loop completed with size 255016, expected 255016

MD5 hexdump of downloaded data:
00000000 AE 1E E3 BC FB AA 51 24 E5 88 A9 01 F2 95 E2 CC |......Q$........|

MD5 hexdump of flashed data:
00000000 AE 1E E3 BC FB AA 51 24 E5 88 A9 01 F2 95 E2 CC |......Q$........|

OTA image was downloaded successfully.
$ image info

Image 0; name APP; state Permanent:
Slot 0; slotAddr 30040000; slotSize 2097152
<EMPTY>
Slot 1; slotAddr 30240000; slotSize 2097152
<IMAGE APP_SECONDARY: size 253656; version 1.18.0.0>
$ image test 0

write magic number offset = 0x43ff00

$ image info

Image 0; name APP; state ReadyForTest:
Slot 0; slotAddr 30040000; slotSize 2097152
<EMPTY>
Slot 1; slotAddr 30240000; slotSize 2097152
<IMAGE APP_SECONDARY: size 253656; version 1.18.0.0>
$ reboot

System reset!
hello sbl.

Disabling flash remapping function
Bootloader Version 1.10.0

Image 0 Primary slot: Image not found

Secondary slot: version=1.18.0+0

Found a candidate in slot 1
writing copy_done; fa_id=1 off=0x1fffe0 (0x43ffe0)

Image 0 loaded from the secondary slot

Bootloader chainload address offset: 0x240000

Reset_Handler address offset: 0x240400

Jumping to the image

Booting the secondary slot - flash remapping is enabled

OTA HTTPS client demo (Ethernet)

Initializing PHY...

Obtaining IP address from DHCP...

************************************************

OTA HTTPS Client Example

************************************************

IPv4 Address : 10.1.15.164

IPv4 Subnet mask : 255.255.255.0

IPv4 Gateway : 10.1.15.1

************************************************

Copyright 2022 NXP

$ image info

Image 0; name APP; state Testing:
Slot 0; slotAddr 30040000; slotSize 2097152
<EMPTY>
Slot 1; slotAddr 30240000; slotSize 2097152
<IMAGE APP_SECONDARY: size 253656; version 1.18.0.0>
$ hello sbl.

Disabling flash remapping function
Bootloader Version 1.10.0

Image 0 Primary slot: Image not found

Secondary slot: version=1.18.0+0

Erasing faulty image in the secondary slot.

No slot to load for image 0

Unable to find bootable image

 

标签 (1)
标记 (2)
0 项奖励
回复
1 解答
3,285 次查看
Gavin_Jia
NXP TechSupport
NXP TechSupport

Hi @drb55 ,

I'm sorry for the trouble this error has caused you, and for that I sincerely apologize. And thank you for pointing out this discrepancy.

I received a response from the internal team regarding this issue:

This difference is due to the use of the remap function. For platforms like RT1050 and RT1020, they do not have a remap function, so mcuboot needs to move the image from slot2 to slot1. but for platforms that support the remap function, you can choose which slot to jump to by simply enabling or disabling the remap function. Due to the SDK readme generation mechanism, it caused the doc issue.

In the meantime, the issue has been reported and will be fixed in a later released version.

Wish you a nice day.

Best regards,
Gavin

 

 

在原帖中查看解决方案

0 项奖励
回复
8 回复数
3,460 次查看
Gavin_Jia
NXP TechSupport
NXP TechSupport

Hi @drb55 ,

Thanks for your interest in NXP MIMXRT series!

I have tested with RT1060EVK on my side, it should be same as RT1170 except the flash address.

Please confirm a few points:

1. Signed application images directly programmed into flash memory by a programmer require additional "--pad --confirm" parameter for imgtool. This parameter adds additional trailer to the signed image and is required by bootloader direct-xip process (see MCUBoot documentation for more information). Signed images used in OTA process do not require "-pad" parameter.

2. Use Jlink to flash the signed client's image to flash at address 0x3004_0000 instead of 0x3004_0400.

I read your log and found that slot0 is always EMPTY, which is not correct.

Gavin_Jia_0-1718348058659.png

Here is my log:

Gavin_Jia_1-1718348121166.png

 

Following the steps should result in good news.

Best regards,
Gavin

0 项奖励
回复
3,454 次查看
drb55
Contributor III

Hi,

Updated as you suggested, and a different message occurs. Images built without padding and Release configuration.

 

OTA HTTPS client demo (Ethernet)

Initializing PHY...

Obtaining IP address from DHCP...

************************************************

OTA HTTPS Client Example

************************************************

IPv4 Address : 10.1.15.179

IPv4 Subnet mask : 255.255.255.0

IPv4 Gateway : 10.1.15.1

************************************************

Copyright 2022 NXP

$ hello sbl.

Disabling flash remapping function
Bootloader Version 1.10.0

Primary slot: version=1.6.0+0

Secondary slot: version=1.7.0+0

Image 0 loaded from the secondary slot

Bootloader chainload address offset: 0x240000

Reset_Handler address offset: 0x240400

Jumping to the image

Booting the secondary slot - flash remapping is enabled

OTA HTTPS client demo (Ethernet)

Initializing PHY...

Obtaining IP address from DHCP...
************************************************

OTA HTTPS Client Example

************************************************
IPv4 Address : 10.1.15.179

IPv4 Subnet mask : 255.255.255.0

IPv4 Gateway : 10.1.15.1

************************************************

Copyright 2022 NXP

$ image info

Image 0; name APP; state Permanent:
Slot 0; slotAddr 30040000; slotSize 2097152
<IMAGE APP_PRIMARY: size 303792; version 1.6.0.0>
Slot 1; slotAddr 30240000; slotSize 2097152
<IMAGE APP_SECONDARY: size 303792; version 1.7.0.0>
$ image test 0

write magic number offset = 0x23ff00

$ image info

Image 0; name APP; state ReadyForTest:
Slot 0; slotAddr 30040000; slotSize 2097152
<IMAGE APP_PRIMARY: size 303792; version 1.6.0.0>
Slot 1; slotAddr 30240000; slotSize 2097152
<IMAGE APP_SECONDARY: size 303792; version 1.7.0.0>
$ hello sbl.

Disabling flash remapping function
Bootloader Version 1.10.0

Primary slot: version=1.6.0+0

Secondary slot: version=1.7.0+0

Found a candidate in slot 0
writing copy_done; fa_id=0 off=0x1fffe0 (0x23ffe0)

Image 0 loaded from the primary slot

Bootloader chainload address offset: 0x40000

Reset_Handler address offset: 0x40400

Jumping to the image

Booting the primary slot - flash remapping is disabled

OTA HTTPS client demo (Ethernet)

Initializing PHY...

Obtaining IP address from DHCP...

************************************************

OTA HTTPS Client Example

************************************************

IPv4 Address : 10.1.15.179

IPv4 Subnet mask : 255.255.255.0

IPv4 Gateway : 10.1.15.1

************************************************

Copyright 2022 NXP

$ image info

Image 0; name APP; state Testing:
Slot 0; slotAddr 30040000; slotSize 2097152
<IMAGE APP_PRIMARY: size 303792; version 1.6.0.0>
Slot 1; slotAddr 30240000; slotSize 2097152
<IMAGE APP_SECONDARY: size 303792; version 1.7.0.0>


$ image accept 0

Deleting header of inactive image in secondary slot (downgrade support for direct-xip)


$ image info

Image 0; name APP; state Permanent:
Slot 0; slotAddr 30040000; slotSize 2097152
<IMAGE APP_PRIMARY: size 303792; version 1.6.0.0>
Slot 1; slotAddr 30240000; slotSize 2097152
<EMPTY>

0 项奖励
回复
3,416 次查看
Gavin_Jia
NXP TechSupport
NXP TechSupport

Hi @drb55 ,

I think your operation should be successful. How do you tell if the operation was successful? By the version information of the two images? I don't see reboot in your second operation. 

For me, the distinction is made by two identical IMAGES, with only the difference in print information.(V1 or V2)

image test 0 --> reboot --> image --> image accept 0

On the success of the Reboot step, the candidate image is executed. The subsequent steps are simply to remove the header of the inactive IMAGE.

Gavin_Jia_0-1718606389446.png

 

Best regards,
Gavin

0 项奖励
回复
3,389 次查看
drb55
Contributor III

Hi,

Based on your suggestions I now have images in both slots. Why does the Bootloader boot from the image in the Secondary Slot and delete header of inactive image in primary slot (downgrade support for direct-xip) instead of moving the image in the Secondary Slot to the Primary Slot?

The Readme document says the image in the Secondary Slot should be moved to the Primary Slot.

  1. After new image is installed and booted, again use the 'image' command to make sure that the image moved from secondary slot into primary slot and image state is now set as "Testing".

Can you explain the discrepancy between the documentation and the actual result?

 

Disabling flash remapping function

Bootloader Version 1.10.0

Primary   slot: version=2.1.0+0

Image 0 Secondary slot: Image not found

Found a candidate in slot 0

writing copy_done; fa_id=0 off=0x1fffe0 (0x23ffe0)

Image 0 loaded from the primary slot

Bootloader chainload address offset: 0x40000

Reset_Handler address offset: 0x40400

Jumping to the image

Booting the primary slot - flash remapping is disabled

OTA HTTPS client demo  V1V1V1 (Ethernet)

Initializing PHY...

Obtaining IP address from DHCP...

************************************************

OTA HTTPS Client Example

************************************************

IPv4 Address     : 10.1.15.110

IPv4 Subnet mask : 255.255.255.0

IPv4 Gateway     : 10.1.15.1

************************************************

Copyright  2022  NXP

$ image info

Image 0; name APP; state None:

  Slot 0; slotAddr 30040000; slotSize 2097152

    <IMAGE APP_PRIMARY: size 253664; version 2.1.0.0>

  Slot 1; slotAddr 30240000; slotSize 2097152

    <EMPTY>

$ ota 0 /ota.bin 10.1.15.119 4433

Started OTA with:

    image = 0

    file = /ota.bin

    host = 10.1.15.119

    port = 4433

  . Seeding the random number generator...

  . Loading the CA root certificate... ok (0 skipped)

  . Loading the client cert. and key... ok

  . Connecting to 10.1.15.119:4433

  . Setting up the SSL/TLS structure... ok

  . SSL state connect : 0

  . Performing the SSL/TLS handshake...

    [ Protocol is TLSv1.2 ]

    [ Ciphersuite is TLS-ECDHE-RSA-WITH-AES-256-GCM-SHA384 ]

    [ Record expansion is 29 ]

  . Verifying peer X.509 certificate... SKIPPED

Getting size of requested file '/ota.bin'

Determined file size is 255024 bytes

Starting download of 255024 bytes with block size of 4096 bytes

...............................................................

Download loop completed with size 255024, expected 255024

MD5 hexdump of downloaded data:

00000000  D0 B2 1D E5 3E CD 0C EE D5 DE 5B D3 4B F5 95 49 |....>.....[.K..I|

MD5 hexdump of flashed data:

00000000  D0 B2 1D E5 3E CD 0C EE D5 DE 5B D3 4B F5 95 49 |....>.....[.K..I|

OTA image was downloaded successfully.

$ image info

Image 0; name APP; state None:

  Slot 0; slotAddr 30040000; slotSize 2097152

    <IMAGE APP_PRIMARY: size 253664; version 2.1.0.0>

  Slot 1; slotAddr 30240000; slotSize 2097152

    <IMAGE APP_SECONDARY: size 253664; version 2.2.0.0>

$ image test 0

write magic number offset = 0x43ff00

$ image info

Image 0; name APP; state ReadyForTest:

  Slot 0; slotAddr 30040000; slotSize 2097152

    <IMAGE APP_PRIMARY: size 253664; version 2.1.0.0>

  Slot 1; slotAddr 30240000; slotSize 2097152

    <IMAGE APP_SECONDARY: size 253664; version 2.2.0.0>

$ hello sbl.

Disabling flash remapping function

Bootloader Version 1.10.0

Primary   slot: version=2.1.0+0

Secondary slot: version=2.2.0+0

Found a candidate in slot 1

writing copy_done; fa_id=1 off=0x1fffe0 (0x43ffe0)

Image 0 loaded from the secondary slot

Bootloader chainload address offset: 0x240000

Reset_Handler address offset: 0x240400

Jumping to the image

Booting the secondary slot - flash remapping is enabled

OTA HTTPS client demo  V2V2V2 (Ethernet)

Initializing PHY...

Obtaining IP address from DHCP...

************************************************

OTA HTTPS Client Example

************************************************

IPv4 Address     : 10.1.15.110

IPv4 Subnet mask : 255.255.255.0

IPv4 Gateway     : 10.1.15.1

************************************************

Copyright  2022  NXP

$ image info

Image 0; name APP; state Testing:

  Slot 0; slotAddr 30040000; slotSize 2097152

    <IMAGE APP_PRIMARY: size 253664; version 2.1.0.0>

 Slot 1; slotAddr 30240000; slotSize 2097152

    <IMAGE APP_SECONDARY: size 253664; version 2.2.0.0>

$ image accept 0

Deleting header of inactive image in primary slot (downgrade support for direct- xip)

$ hello sbl.

Disabling flash remapping function

Bootloader Version 1.10.0

Image 0 Primary slot: Image not found

Secondary slot: version=2.2.0+0

Image 0 loaded from the secondary slot

Bootloader chainload address offset: 0x240000

Reset_Handler address offset: 0x240400

Jumping to the image

Booting the secondary slot - flash remapping is enabled

OTA HTTPS client demo  V2V2V2 (Ethernet)

Initializing PHY...

Obtaining IP address from DHCP...

************************************************

OTA HTTPS Client Example

************************************************

IPv4 Address     : 10.1.15.110

IPv4 Subnet mask : 255.255.255.0

IPv4 Gateway     : 10.1.15.1

************************************************

Copyright  2022  NXP

$ image info

Image 0; name APP; state Permanent:

  Slot 0; slotAddr 30040000; slotSize 2097152

    <EMPTY>

  Slot 1; slotAddr 30240000; slotSize 2097152

    <IMAGE APP_SECONDARY: size 253664; version 2.2.0.0>

$

0 项奖励
回复
3,356 次查看
Gavin_Jia
NXP TechSupport
NXP TechSupport

Hi,

Thanks for pointing this out. I am consulting with internal team and will keep you updating in this thread.

Best regards,
Gavin

0 项奖励
回复
3,349 次查看
drb55
Contributor III

Hi,

Does anyone in development actually read the documentation and readme files for accuracy or is NXP hoping the customers will find the errors and point them out.

0 项奖励
回复
3,286 次查看
Gavin_Jia
NXP TechSupport
NXP TechSupport

Hi @drb55 ,

I'm sorry for the trouble this error has caused you, and for that I sincerely apologize. And thank you for pointing out this discrepancy.

I received a response from the internal team regarding this issue:

This difference is due to the use of the remap function. For platforms like RT1050 and RT1020, they do not have a remap function, so mcuboot needs to move the image from slot2 to slot1. but for platforms that support the remap function, you can choose which slot to jump to by simply enabling or disabling the remap function. Due to the SDK readme generation mechanism, it caused the doc issue.

In the meantime, the issue has been reported and will be fixed in a later released version.

Wish you a nice day.

Best regards,
Gavin

 

 
0 项奖励
回复
3,218 次查看
drb55
Contributor III

Hi,

I think it would have been better to publish accurate documentation instead of me wasting my time asking a question and you answering a question which is probably unnecessary but that's just my opinion. Hoping for better documentation from NXP in the future, not holding my breath.

0 项奖励
回复