error in booting of freeRTOS

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

error in booting of freeRTOS

620 次查看
SAURAVMISHRA95
Contributor I

BSP version:-

PRETTY_NAME="NXP Real-time Edge Distro 3.1 (scarthgap)"
CPE_NAME="cpe:/o:openembedded:nxp-real-time-edge:3.1"

Error: No resource table in freertos_hello_cm7.elf 

following error is coming while booting:-

root@imx8mp-lpddr4-evk:~# echo start > /sys/class/remoteproc/remoteproc0/state[ 1781.905171] remoteproc remoteproc0: powering up imx8mp-cm7
[ 1781.910070] remoteproc remoteproc0: Booting fw image freertos_hello_cm7.elf, size 256200
-sh: echo: write error: Invalid a[ 1781.910115] remoteproc remoteproc0: header-less resource table
rgument[ 1781.910120] remoteproc remoteproc0: No resource table in elf

[ 1781.910168] imx-rproc imx8mp-cm7: Translation failed: da = 0x7e0000 len = 0x2a8
[ 1781.910175] remoteproc remoteproc0: bad phdr da 0x7e0000 mem 0x2a8
[ 1781.910183] remoteproc remoteproc0: Failed to load program segments: -22
root@imx8mp-lpddr4-evk:~# [ 1781.910252] remoteproc remoteproc0: Boot failed: -22

标签 (1)
0 项奖励
回复
3 回复数

598 次查看
JosephAtNXP
NXP TechSupport
NXP TechSupport

Hi,

Thank you for your interest in NXP Semiconductor products,

Are you building RT Edge Software from this website? Are you performing any changes on SW?

Could you try to replicate with prebuilt images and steps from Users Guide?

Regards

0 项奖励
回复

577 次查看
SAURAVMISHRA95
Contributor I

we have already followed the step mentioned above.while running the demo examples of freeRTOS hello world we are receiving the error mentioned above.

0 项奖励
回复

506 次查看
JosephAtNXP
NXP TechSupport
NXP TechSupport

Hi,

Please share the steps, if possible, the chapter that you are setting up to reproduce on my side,

Regards

0 项奖励
回复