BSP version:-
PRETTY_NAME="NXP Real-time Edge Distro 3.1 (scarthgap)"
CPE_NAME="cpe:/o:openembedded:nxp-real-time-edge:3.1"
Error: No resource table in freertos_hello_cm7.elf
following error is coming while booting:-
root@imx8mp-lpddr4-evk:~# echo start > /sys/class/remoteproc/remoteproc0/state[ 1781.905171] remoteproc remoteproc0: powering up imx8mp-cm7
[ 1781.910070] remoteproc remoteproc0: Booting fw image freertos_hello_cm7.elf, size 256200
-sh: echo: write error: Invalid a[ 1781.910115] remoteproc remoteproc0: header-less resource table
rgument[ 1781.910120] remoteproc remoteproc0: No resource table in elf
[ 1781.910168] imx-rproc imx8mp-cm7: Translation failed: da = 0x7e0000 len = 0x2a8
[ 1781.910175] remoteproc remoteproc0: bad phdr da 0x7e0000 mem 0x2a8
[ 1781.910183] remoteproc remoteproc0: Failed to load program segments: -22
root@imx8mp-lpddr4-evk:~# [ 1781.910252] remoteproc remoteproc0: Boot failed: -22